FSCI Messages XML#
Overview#
The Framework Serial Communication Interface (FSCI) module supports interfacing the BLE Host Stack with a host or a PC tool (Test Tool for Connectivity Products) using a serial communication line. If the FSCI is used with the NXP Test Tool for Connectivity products, the tool can use an XML file containing a detailed meta-description for serial commands and events. This XML file is provided in the software packages that include this document.
Bluetooth LE Host Stack interface set
The Bluetooth LE Host Stack layers that offer access using FSCI are L2CAP, L2CAP CB, GATT, GATTDB, GAP, FSCI, and NVM. Each layer provides primitives that an upper layer (profile/application) uses to access services of that layer. This document includes a detailed list of the provided primitives.
Basic requirements
Following are the hardware requirements for using FSCI API RM:
IAR Embedded Workbench for Arm architecture
NXP development boards (to be loaded with the ble_fscibb application)
Optional Bluetooth LE sniffer for testing
PC tool (Test Tool for Connectivity Products) or another host processor capable of communicating through UART, USB, SPI, or I2C
FSCI message description#
This chapter describes the L2CAP, L2CAP CB, GATT, GATTDB, GAP, FSCI, and NVM commands (requests) and events (confirms and indications) in detail.
The BLE.xml document is found in the ble_fsci_app subfolder, and provides an XML representation of all these commands and events.
The BLE_x.x.x.xml document is found in the ..\tools\wireless\xml_fsci\ subfolder, and provides an XML representation of all these commands and events.
How to interpret the XML
The XML is structured in <Commands> and <Events> tags, the contents grouped by layer. Each group contains the description <GroupDesc> and multiple <Cmd> tags (as shown below).
<BLE>
<Commands>
<L2CAP>
<GroupDesc>L2CAP Commands</GroupDesc>
<Cmd>
<CmdName>L2CAP-Init.Request</CmdName>
<CmdDesc>L2CAP initialization function</CmdDesc>
<CmdHeader>41 01</CmdHeader>
<CmdParms>
</CmdParms>
</Cmd>
[...]
</L2CAP>
<L2CAPCB>
[...]
</L2CAPCB>
[...]
</Commands>
<Events>
[...]
</Events>
[...]
</BLE>
Every command or event is described in a <Cmd> that contains:
the name -
<CmdName>the description -
<CmdDesc>the opGroup and opCode -
<CmdHeader>the parameters -
<CmdParms>
The parameters of a command/event are specified using the <Parm> tag and contain:
the name -
<ParmName>the description -
<ParmDesc>the size -
<ParmSize>the type -
<ParmType>the last value -
<ParmLastValue>the default value -
<ParmDefaultValue>the type specifics -
<ParmTypeSpecifics>
The type specifics tag is used where needed to specify certain behaviours:
<ParmItem>for specifying enum items<ParmState>for specifying the state of a variable (e.g. ReadOnly)<ParmRange>for specifying the range of the values taken by a variable<Depend>for specifying a dependence on another variable (e.g.an array’s dependence on the length variable)<Parm>for specifying the parameters of a struct
FSCI message example#
For example, the L2CAP-SendAttData.Request command has the following XML structure:
<Cmd>
<CmdName>L2CAP-SendAttData.Request</CmdName>
<CmdDesc>Sends a data packet through ATT Channel</CmdDesc>
<CmdHeader>41 03</CmdHeader>
<CmdParms>
<Parm>
<ParmName>DeviceId</ParmName>
<ParmDesc>The DeviceId for which the command is intended</ParmDesc>
<ParmSize>1</ParmSize>
<ParmType>tInt</ParmType>
<ParmLastValue>00</ParmLastValue>
<ParmDefaultValue>00</ParmDefaultValue>
</Parm>
<Parm>
<ParmName>PacketLength</ParmName>
<ParmDesc>Length of the ATT data packet to be sent</ParmDesc>
<ParmSize>2</ParmSize>
<ParmType>tInt</ParmType>
<ParmLastValue>0001</ParmLastValue>
<ParmDefaultValue>0001</ParmDefaultValue>
<ParmTypeSpecifics>
<ParmRange>0x0001-0xFFFF</ParmRange>
</ParmTypeSpecifics>
</Parm>
<Parm>
<ParmName>Packet</ParmName>
<ParmDesc>The ATT data packet to be transmitted</ParmDesc>
<ParmSize>1</ParmSize>
<ParmType>tArray</ParmType>
<ParmLastValue>00</ParmLastValue>
<ParmDefaultValue>00</ParmDefaultValue>
<ParmTypeSpecifics>
<Depend>
<DependName>PacketLength</DependName>
<DependMask>0xFFFF</DependMask>
<DependShift>0x0000</DependShift>
</Depend>
</ParmTypeSpecifics>
</Parm>
</CmdParms>
</Cmd>
This translates to:
Tag |
Value |
Description |
|---|---|---|
|
L2CAP-SendAttData.Request |
Name of the command/event |
|
Sends a data packet through ATT Channel |
Description of the command/event |
|
41 03 |
opGroup and opCode of the command/event in hexadecimal format |
|
|
List of the parameters used in the command/event |
|
DeviceId |
Name of the parameter |
|
The DeviceId for which the command is intended |
Description of the parameter |
|
1 |
Parameter size (in bytes) |
|
tInt |
Type of the parameter |
|
00 |
Last value of the parameter in hexadecimal format |
|
00 |
Default value of the parameter in hexadecimal format |
|
|
Specify range of the parameter |
|
Specify dependency of the parameter “Packet” of type “tArray” of the variable |
Parent topic: Bluetooth Low Energy Host Stack FSCI Application Programming