MCUXpresso SDK Documentation

Changelog

Changelog#

All notable changes to NXP Bluetooth LE Host will be documented in this file.

NXP Bluetooth LE Host Stack is certified Bluetooth 6.0

[1.10.22] - mcux v2026-09-00-pvw2#

Added#

  • Added gSecEvt_SameConfirmValue_c IDS event to detect Legacy Pairing Confirm Value replay attacks

Improved#

  • Replaced mode assert with graceful drop and cleanup in localization applications

  • RAS/RAP: handle case where MTU size reduction forces use of more segments than predefined gRASMaxNoOfSegments_c

  • Advertising-set-related BLE Host storage is now allocated by the application and scales with the configurable gMaxAdvSets_c

Fixed#

  • Fixed CS measurement not starting after handover in digital_key_car_anchor_cs

  • Fixed Insufficient Encryption returned instead of Insufficient Authentication

  • Fixed RSSI filter not excluding invalid RSSI values in CCC monitoring

  • Fixed missing CCC characteristics in digital_key_car_anchor_cs example

  • Fixed mismatch between ExtendedFeatures from GAPInit and HCI LE Read All Remote Features Complete event

  • Miscellaneous Sample Applications fixes

  • Miscellaneous Coverity fixes

  • Miscellaneous MISRA fixes

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23, KW43, MCXW70

[1.10.21] - mcux v2026-09-00-pvw1#

Added#

  • RSSI-based adaptive CS procedure interval for localization applications (experimental; disabled by default)

  • Added BTCS timer mechanism to ensure CS procedure loop restarts are not blocked by failed L2CAP transfers

Improved#

  • CS procedure parameters are now updated on connection interval change to avoid CS request rejection

  • Aligned wireless_uart preinclude settings across all platforms for consistency

  • Updated ble_shell periodic advertising default interval set to 1 second for improved discoverability

  • Increased host task stack size across multiple applications

  • Extended ble_shell periodic advertising handling to support gPeriodicDeviceScannedV2_c event

  • RADE component naming updated in documentation

  • Unified CS results complete event handling; real-time transfer moved to AppLocalization_HandleCompleteResults()

Fixed#

  • Fixed out-of-bounds access in gap.c

  • HCI LE Read All Remote Features command is now issued if supported by the controller

  • Power Control APIs now return gBleFeatureNotSupported_c if the controller does not indicate support

  • Fixed array index overflow in application ranging_client.c

  • Fixed local RSSI parsing: correct byte is now collected before advancing parse pointer

  • Fixed bounds check for gaAntPermNAp in processMode2Data and processMode3Data

  • Fixed localization index overflow; added sanity check

  • Corrected bounds check for deviceId

  • Fixed wireless_uart mAdvPending flag to prevent multiple advertising starts during multi-peer disconnect

  • Fixed missing RSSI variables causing compilation issues in app_localization_utils.c

  • TPMS sensor Signing Key and sequence number now saved in NVM to prevent MAC check failures

  • CS IPT mode now configured with only 1 antenna path to fix Samsung phone CS request rejection

  • FSCI Extended NBU: Added LL_API_NotifyWakeUp call in idle_task to detect NBU stuck condition; added leExtendedFeatures to NCP GAP init complete event

  • Fixed systick drift when PWR_DisallowDeviceToSleep() is active

  • CS: Added check for valid numAntennaPaths in processCsResultsEvent

  • Miscellaneous MISRA fixes

  • Miscellaneous Coverity fixes

Changed#

  • Reverted incorrect connection handle handling for non-connection enhanced notification events

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23, KW43, MCXW70

[1.10.20] - mcux v2026-06-00#

Added#

  • Tire Pressure Monitoring System (TPMS) sample demo applications (KW4x)

  • Tire Pressure Monitoring System (TPMS) documentation added to DAUG

  • Localization accelerator LCE support for KW43/MCXW70

  • Added LE Power Control support in BLE Shell application

  • LE Read All Remote Features (LLEFS) support in HOST-GAP

  • LE Channel Assessment (CHAS) Config HCI command support in HOST-GAP

  • Sensor support enabled on KW43/MCXW70

Improved#

  • CS procedure auto-loop shell command; improved RAS data drop mechanism

  • Allow ‘setnumprocs’ 0 for infinite CS procedure repeats

  • Synchronize code between loc_reader and ncp_loc_reader application files

  • Subevent interval added to RADE algoritm API

  • Updated connection handover setup info for FRDM-KW43 in CS application documentations

  • Documentation updates

Fixed#

  • L2CAP data fragmentation fix causing inccorect fragmentation over the air

  • Fix for no valid subevents in localization

  • Allow sub_mode_type 255 in CS config params

  • Incorrect connection handle (0 instead of 0xFFFF) for non-connection enhanced notification events

  • Channel Sounding subevent abort (No CS_SYNC mode0) after rebond

  • Set ‘preferredPeerAntenna’ based on peer capabilities

  • Miscellaneous minor application bug fixes

Changed#

  • Reduced cyclomatic complexity (CCM) in multiple localization functions

  • Decoupled buttons from LEDs in Bluetooth applications

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23, KW43, MCXW70

[1.10.19] - mcux v2026-06-00-pvw2#

Added#

  • Support for LE Read All Remote Features after connection is established

  • Experimental Inline PCT Transfer support for localization sample applications

  • Support for configurable limits for concurrent Channel Sounding connections/procedures

Improved#

  • Optimized memory allocation in isp_mciq_ranging_compute for localization applications

  • Updated RAS loc_reader application for multiple CS connections

  • Updated handover documentation with broadcast time synchronization details

  • Documentation updates

Fixed#

  • Fixed double free issue in L2ca_SendAclDataWithSegmentation

  • Fixed consecutive CS procedures sustainability issue

  • Miscellaneous minor application bug fixes

Changed#

  • CS procedure state management: do not allow new procedure to start before previous one completes

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23, KW43

[1.10.18] - mcux v2026-06-00-pvw1#

Added#

  • Support for RTT 0 m calibration in applications.

  • Support for CS Enhancements at Host level:

    • Inline PCT Transfer

    • RTT 2M PHY

  • New connection event ‘gConnEvtRemoteFeaturesRead_c’, providing the peer feature bitmask read via the Read Remote Features procedure

  • Support for 5 advertising sets in the Bluetooth LE Host

  • Method to specify GATT handles on the client, avoiding repeated service discovery

  • Slope calibration algorithm for CS (experimental, disabled by default). Computes distance and quality indicators per antenna path

  • Handover broadcast time synchronization, allowing one connected anchor to synchronize multiple target anchors simultaneously

  • Added common configuration header ‘app_localization_config.h’, overridable by the user

Improved#

  • Updated handling of ‘Procedure_Results_Start’ to correctly process multiple subevents in a single message

  • Improved CS temperature polling mechanism

  • BTCS Server now explicitly notifies the PSM channel via ‘AppLocalization_SetPsmChannelId’ upon handover connection

  • RAS/BTCS clients can disable algorithm execution via ‘gRunAlgo_d’

  • Updated and cleaned ‘app_preinclude.h’ for sample applications

  • Documentation and configuration updates for LCE enable/disable

  • Documentation updates

  • Miscellaneous minor application bug fixes

Fixed#

  • If the LE Set Periodic Adv Subevent Data command finishes with an error, use ‘gInternalError_c’ with ‘gLeSetPeriodicAdvSubeventData_c’ as the source and the command complete status as the error code

  • Correct handling of AddrType values in MonAdvReport generated from XML

Changed#

  • Removed the Bluetooth LE Host library from the wireless_uart_host project

  • Disabled use of Random Static Address for all applications except: digital_key_car_anchor and digital_key_car_anchor_cs

  • Set maximum CS procedure duration to: (procedure interval x connection interval x 2 - 1) slots

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.17] - mcux v2026-03-00#

Added#

  • Test mode functionality for the Intrusion Detection System

  • GAP API for HCI LE_Set_Local_Slave_Latency_Enable vendor command

  • gRasUseNotifOrInd_c to allow configuration of Indication or Notification on RAS

  • cs_sync_phy argument to setcsconfig shell command

  • snr_control_init and snr_control_refl arguments to setcsproc shell command

  • Detailed description for setcsconfig and setcsproc command arguments to the CCC w/ CS and Localization applications notes

  • Mode0 step information parsing for both RAS and BTCS, made available for the export module

Improved#

  • ATT Write Commands can now be sent at any time, as per specification

  • Enhanced CCC and RAS Channel Sounding by incorporating real-time local and remote data decompression

  • Localization applications now record the PHY used for establishing the connection and incorporate it into the CS procedure parameters configuration

  • Localization applications keep the subevtStopIdx for the remote data and provide it to the algorithm

  • Localization applications now pass remote mode map to algorithm

  • Eliminated the dependency on hci_interface.h in localization files

  • Documentation updates

  • Miscellaneous minor application bug fixes

Fixed#

  • Wrong data field type in GAP2GenericEventVendorSpecificDebugFatalError

  • Localization application now processes CS results only when local data is available

  • Digital key car anchor application issue related to setting the GAP role prior to any use

  • Error in the definition of a CCC PSM VDBT Version GATT characteristic

  • Issue with PACKET_NADM byte not being packed correctly into the TOF buffer for mode-3 steps

  • MISRA fixes

Changed#

  • Modified linker section names, comments, and RAM layout in the connectivity.icf and connectivity_ble_loc.ld files for every KW47 and MCXW72 board

  • Set the default CS submode and default rtt_type to 3

  • Set the default radio core speed for the Channel Sounding application to 48 MHz

  • Localization applications configured to use the extended heap as the final segment of DATA1

  • Deleted the gcGapMaximumActiveConnections_c definition from applications

  • Eliminated unused fields related to CS Test Mode

  • Deleted initializations of range settings that were subsequently overwritten

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.16] - mcux v2026-03-00-pvw2#

Added#

  • Implemented Bluetooth LE Host Transient Application Key feature (experimental). in ble_shell, loc_reader and loc_user_device

  • Added Bluetooth LE Host Transient Application Key in ble_shell, loc_reader and loc_user_device

  • Added Channel Sounding phase calibration, with 0.5m compensation for all boards

  • Added Vendor Specific Command to enable Link Layer experimental features

  • Added gAppCsTimeInfo_d define in app_preinclude.h for digital_key_car_anchor_cs on KW47EVK

  • Added Channel Sounding phase calibration logic and updates in RAS CS Procedure Timing Measurement

Improved#

  • Updated RADE algorithm source files license description with NXP proprietary license

  • Improved data logging for digital key application

  • Updated CCC enumeration values to align with CCC v4.0.0 specification

  • Updated Intrusion Detection System documentation with event details

  • Documentation miscellaneous updates

Fixed#

  • Fixed ranging data body parser on the client side — aborted steps are now counted correctly to prevent subevent misalignment

  • Fixed handling of CS Procedure Disable at Host and application level

  • Fixed app_localization timer blocking when sensors were disabled

  • Fixed setting of gCsTimeInfo.transferStart for BTCS Client L2CAP transfer

  • Removed unused gAppRealTimeDataTransfer_c define from digital_key_car_anchor_cs

  • Removed pin_mux files from core1 application projects

  • Fixed issues in data transfer and event updates related to timing measurement

Changed#

  • Updated (SHELL_MAX_ARGS = 20) in app_preinclude.h for localization applications.

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.15] – mcux v2026-03-00-pvw1#

Added#

  • Added an API to update local synchronization parameters after PAwR is already established on the scanner side

  • Added Connection Subrating feature (experimental) in the Bluetooth LE Host

  • Added Connection Subrating feature in ble_shell

  • CCC v4.1.0: renamed DK_VERSION to VDBT_VERSION as per updated specification

Improved#

  • Improved localization applications timer mechanism to reduce the number of wakeups

  • Updated localization timeout values to be overridable by the application

  • Retain the subevent_done_status local and remote values for all subevents and pass them to the algorithm

  • Documentation miscellaneous updates

Fixed#

  • Fixed L2CAP credit-based channel disconnection where the channel’s timer ID would be set to 0 instead of gTmrInvalidTimerID_c

  • Fixed Channel Sounding applications issue: clear the Indication Pending flag for a peer device on disconnect

  • ble_shell: Set maximum arguments in command (SHELL_MAX_ARGS = 20) in app_preinclude.h

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.14] - mcux v2025-12-00#

Added#

  • KW47/MCXW72 CCC and IOT Channel Sounding Localization applications on GitHub repository

  • Monitoring Advertisers support in fsci_black_box and BleShell applications

  • Local average and remote average RSSI values to the CS measurement report

  • The “-Os” optimization flag to the ARMGCC release configuration for NCP applications

Improved#

  • Enabled low power support in loc_reader_host application

Fixed#

  • loc_reader_host application event set issue

  • Missing handler for Version2 of the Set RPA Timeout command

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.13] - mcux v2025-12-00-pvw2#

Added#

  • Threshold for the invalid number of Anchor Monitor events received by the target anchor

  • Experimental Monitoring Advertisers feature in Bluetooth LE Host

  • Experimental Randomized RPA feature in Bluetooth LE Host

  • Application defines for default connection and default advertising tx power

Improved#

  • Miscellaneous applications updates

  • Central applications now wait for status of Encrypt procedure in case of bonded device

  • Logging data on localization applications

  • NBU Low Power Mode enabled by default for Localization Applications

  • PCT rotation calibration added to localization apps

  • Configured CS Reflector to start the CS procedure with the tdm command and updated the documentation

  • Populated the optionalSubfeaturesSupported field correctly

  • Prevented CORE 0 from entering deep sleep while LCE is computing by setting the low power mode constraint to PWR_WFI during LCE computation and releasing it afterwards

  • Implemented in CCC_CS, Channel Sounding data transfer from the anchor to the device

  • Documentation miscellaneous updates

  • Updated all kw47 and kw45 armgcc ld linker files to take gUseInternalStorageLink_d flag value into consideration

Fixed#

  • Memory issue when setting scan response data would return an error status from the LL

  • Set advertises with the public address, overwritten by a previously used random address on receiving the Advertising Set Terminated event

Changed#

  • Updated memory configuration: replaced the extended heap area in the available SMU2 memory with a 24KB array in the data1

  • Removed redundant cached remote capabilities write on reflectors, as the initiator will always trigger a capabilities exchange and trying to write cached capabilities afterwards results in an HCI error

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.12] - mcux v2025-12-00-pvw1#

Added#

  • Gap_LoadCustomBondedDeviceInformation API to retrieve custom peer information using NVM index

Improved#

  • Miscellaneous application updates

Fixed#

  • Updated privacy timeout mechanism affected by LE Set Extended Advertising Enable Command

Changed#

  • Merged Gap_SetPeriodicAdvParameters and Gap_SetPeriodicAdvParametersV2 into Gap_SetPeriodicAdvParameters

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.11] - mcux v2025-09-00#

Added#

  • CCC sample applications updated to CCC Digital Key v4.0.0 Specification

  • RAS/RAP PTS 8.7.4 test support added in Localization Sample applications

  • Support for CS start procedure while the previous procedure is not completed; old procedure replaced with the new one

  • Support for arm gcc for ncp_loc_reader__cm33_core1

Improved#

  • Localization Sample Applications Ram partition

  • RAS/RAP profile and service

  • Various sample applications have been updated

Fixed#

  • Privacy setting issue on ncp_loc_reader

  • Extended NBU FSCI message handling issue

  • Ble_shell updated to set the Random Static Address properly

  • Always set the Advertising Legacy Set handle if the legacy API was used

  • fsci_bridge and w_uart_host memory leak

  • PAWR parameters in PeriodicSyncTransferReceived are now parsed correctly

  • Ensure an RPA/NRPA is properly set from the application to enable a central using Controller Privacy to connect to unbonded peripherals

  • CS algorithm buffer overwrite issue during Connection Handover application

  • Various sample applications bug fixes applied

  • Pass correct Codded PHY (S2) to Channel Sounding Set Procedure Parameters

Changed#

  • Merged Gap_SetExtAdvertisingParameters and Gap_SetExtAdvertisingParametersV2 into Gap_SetExtAdvertisingParameters

  • ce_status_buffer type changed to int32_t

  • BLE_Shell prints Random Static address as identity address instead of the Public Device Address

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.10] - mcux v2025-09-00-pvw2#

Improved#

  • CS Event Handling: CS (Channel Sounding) events are now sent to the application task for processing, rather than being handled directly in the Host task

  • Various sample applications have been updated

Fixed#

  • Bluetooth Advertising Sets: Now supports 4 advertising sets in the Bluetooth host libraries

  • Various sample applications bug fixes applied

Changed#

  • Bluetooth Address Type: The default address type has been changed from Public to Random Static

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.9] - mcux v2025-09-00-pvw1#

Added#

  • IDS event trigger when incoming ATT packets exceed agreed MTU

  • IDS event trigger when Unexpected SMP Messages received in idle states (before pairing starts)

  • Average RSSI reporting in Anchor Monitor event

  • Support for gAppDeferAlgoRun_d in btcs_client.c

  • Multi-connection monitoring in Handover/Monitor Mode

Improved#

  • Updated NBU channel sounding applications to support 64MHz clock speed

  • Cleanup of commComplete structures that only contain status from hci_interface.h

Fixed#

  • CCC Application handover monitoring RSSI issue

  • Intrusion Detection System not reporting event type

  • Extended NBU armgcc projects stability

  • Advertising Extended Applications when Gap_PeriodicAdvCreateSync fails

Changed#

  • Updated digital_key_car_anchor applications to configure coding scheme via Host API

  • Enhanced RAS handling of ACK Ranging Data in invalid conditions

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.8] - mcux v2025-06-00#

Added#

  • Gap_SetBondedDeviceName() to set device name using NVM index

  • RAS queue for GATT indications sent

  • gHciStatusBase_c to csError status

  • Option to use statically allocated memory for dynamic GATT database (prevents heap fragmentation)

  • Checks for controller supported features and setting PAST bits accordingly

  • Anchor support to export device data via RAS using gAppHciDataLogExport_d = 2

  • Anchor support to export device local HCI data using gAppHciDataLogExport_d = 1

  • Shell commands to list peer devices and trigger connection handover

  • Define for enabling optional CCC LE Coded PHY advertising

  • cs_sync_phy parameter to mDefaultRangeSettings (renamed from outdated RTTPhy)

Improved#

  • Stack Host now saves the most recently set random address after successful controller response

  • Miscellaneous minor application updates

Fixed#

  • Compilation issue in loc_reader app with real-time RAS transfer

  • CCC application handover state machine race condition

  • CCC resets gCurrentAdvHandle upon connection

  • RAS uses correct bit for data overwrite preference

Changed#

  • Updated Bluetooth LE Host Documentation.

  • BLE_Shell Tx timer interval adjusted for max throughput on 1M PHY

  • CS_ConfigVendorCommand updated with Inline Phase Return field

  • Renamed tx_pwr_phy to phy and removed obsolete rtt_phy field

  • Updated documentation to clarify Controller Privacy restrictions

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, MCXW23

[1.10.7] - mcux v2025-06-00-pvw2#

Added#

  • Support for Bluetooth LE Debug Keys

  • Support for pairing failure reason 0x10 (Busy)

  • Extended NBU Wireless_uart_host battery service

  • Channel Sounding RSSI Information at application level

  • Application support for 4-antenna configuration

Improved#

  • Clean include directives

  • Allow central-only devices to use Gap_EncryptAdvertisingData

  • CSTACK size optimization for RADE using baremetal apps

Fixed#

  • Extended NBU memory leak issues

  • Issues when gAppOtaASyncFlashTransactions_c is set to 0

  • Issue with CS procedure affected by the CS data export

  • Extended NBU Wireless_uart_host privacy

Changed#

  • Updated Bluetooth LE Host Documentation.

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, K32W1

[1.10.6] - mcux v2025-06-00-pvw1#

Added#

  • Encypted Advertising Data support in Extendded Advertising Applications.

  • Support for disable UART for CS applications for low power measurements.

  • Support for LCE (DSPV) non-blocking API integration to RADE.

  • Intrusion Detection System as Experimental.

Improved#

  • L2CAP command length validation to cover all signaling commands.

  • Extended NBU Wireless_uart_host multiple connections support.

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, K32W1

[1.10.5] - mcux v2025-03-00#

Added#

  • MCXW72 Extended NBU support and w_uart_host, fsci_bridge and ncp_fscibb sample applications.

  • L2CAP support for Channel Sounding IQ Sample Transfer in CCC CS sample applications.

  • Bluetooth LE Sample applications for MCX-W71-EVK board.

Changed#

  • Updated FSCI XML file.

  • Updated Bluetooth LE Host Documentation.

Fixed#

  • Cleared the mpRemoteCachedCaps entry when the peer disconnects (CS sample applications).

  • Transfer RAS subscription data during connection handover (CCC CS sample applications).

  • EAD - Updated advertising data length check to ensure encrypted data fits inside one AD.

  • Updated digital_key_car_anchor and digital_key_car_anchor_cs applications to manage Random Static address from the application layer.

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, K32W1

[1.10.4] - mcux v2025-03-00-pvw2#

Added#

  • PAWR support in BLE Shell sample application.

  • PAWR support in adv_ext_peripheral and adv_ext_central sample applications.

  • New sample applications for FRDM-MCXW72.

  • Gap_SetScanningCallback API.

  • Support for handover connection interval update command.

Changed#

  • Updated HID Device for Windows 11 compatibility.

  • Updated CCC demos to Digital Key R4 spec version 1.0.0.

  • Improved RPA resolution at the Host level, now performed synchronously.

  • Enhanced parsing of the CS procedure in Ranging Service.

Fixed#

  • Corrected parsing of the PAST command in FSCI GAP.

  • Fixed scan event reporting in PAST scenario.

  • Added an error case for Gap_SetChannelMap in the generic event handler.

Supported Platforms#

  • KW45, KW47, MCXW71, MCXW72, K32W1