MCUXpresso SDK Documentation

Sensors#

Overview#

The Sensors module provides an API to communicate with the ADC. Two values can be obtained by this module :

  • Temperature value

  • Battery level

The temperature is given in tenths of degrees Celsius and the battery in percentage.

This module is multi-caller, the ADC is protected by a mutex on the resource and by prevententing lowpower (only WFI) during its processing. Platform specific code can be find in fwk_platform_sensors.c/h.

Features#

Manual Measurement#

Calling “SENSORS_GetTemperature()” or “SENSORS_GetBatteryLevel()” function will give the last measured value that was copied to RAM. If you want to refresh this value you must first call the trigger function (SENSORS_TriggerTemperatureMeasurement() / SENSORS_TriggerBatteryMeasurement()) that configures the ADC to perform temperature or battery measurement, then a call to the refresh function (SENSORS_RefreshTemperatureValue() / SENSORS_RefreshBatteryLevel()) will read the returned value from the ADC and save it in RAM. You can run code between these two functions because the ADC won’t give you the value until it’s fully ready.

Important: When a measurement is ongoing, new measurement requests will be dropped. Measurement triggers are only accepted when the measurement state is IDLE. This applies to both temperature and battery measurements to prevent ADC resource conflicts.

Periodic Temperature Measurement#

The Sensors module supports automatic periodic temperature measurements that can be requested from two sources:

1. HOST Requests#

Applications can request periodic temperature measurements using:

SENSORS_TriggerPeriodicTemperatureMeasurement(uint32_t temperature_meas_interval_ms);

2. NBU Requests (wireless_mcu platforms only)#

The NBU (Narrow Band Unit) can request periodic temperature measurements. For more details about NBU temperature requests check NBU Integration Features section bellow.

Periodic Measurement Behavior#

Immediate Trigger: Every periodic request (HOST or NBU) triggers an immediate measurement before starting the interval timer.

Interval Management:

  • Minimum Interval Selection: When both HOST and NBU request periodic measurements, the system uses the shorter interval

  • Dynamic Updates: Changing the interval from either source immediately triggers a new measurement and restarts the timer with the new effective interval

  • Independent Control: HOST and NBU can independently start/stop their periodic requests

One-shot Mode: Setting interval to 0 triggers a single measurement and stops periodic operation for that source.

Usage Examples#

// HOST requests periodic measurement every 100ms
SENSORS_TriggerPeriodicTemperatureMeasurement(100);

// HOST requests one-shot measurement and stops periodic operation
SENSORS_TriggerPeriodicTemperatureMeasurement(0);

Concurrent Requests Behavior#

HOST Interval

NBU Interval

Effective Interval

Notes

200ms

100ms

100ms

NBU interval is shorter

100ms

300ms

100ms

HOST interval is shorter

0 (stopped)

150ms

150ms

Only NBU active

200ms

0 (stopped)

200ms

Only HOST active

0 (stopped)

0 (stopped)

No periodic

Both stopped

Measurement State Management#

The Sensors module uses a state machine to manage ADC resource access:

States:#

  • MEASUREMENT_IDLE: No measurement in progress, ready to accept new requests

  • TMP_MEASUREMENT_ONGOING: Temperature measurement in progress

  • BAT_MEASUREMENT_ONGOING: Battery measurement in progress

Behavior:#

  • Request Acceptance: New measurement requests are only processed when state is MEASUREMENT_IDLE

  • Request Dropping: If a measurement request is made while another measurement is ongoing, the new request is silently dropped

  • State Transitions: State changes from IDLEONGOING when measurement starts, and back to IDLE when measurement completes

  • Recovery Mechanism: For periodic measurements, if a trigger fails due to ongoing measurement, a 1ms retry timer is started

NBU Integration Features#

Platform Support: NBU integration features are only supported on wireless_mcu platforms. These features are not available on RT, mcxw23, and rw61x platforms.

Periodic Temperature Measurement from NBU#

The Sensors module supports automatic periodic temperature measurements triggered by NBU requests. This feature allows the system to automatically measure temperature at regular intervals without manual intervention. This temperature data is used for XTAL32M calibration and Channel Sounding calibration.

How it works:#

  1. NBU Request: The NBU can request periodic temperature measurements by calling the registered callback with a measurement interval

  2. Timer-based Scheduling: A timer manager is used to schedule periodic measurements based on the requested interval

  3. Workqueue Processing: Temperature measurement triggers are processed through the system workqueue to avoid blocking operations

  4. Automatic Refresh: Once a measurement is complete, the next measurement is automatically scheduled

Key Components:#

  • Temperature Request Callback: Sensors_TemperatureReqCb() - Handles NBU requests for periodic measurements

  • Timer Callback: Sensors_TempMeasTimerCallback() - Triggers measurements on timer expiration

  • Work Handler: Sensors_PeriodicTempWorkHandler() - Processes temperature measurement requests in workqueue context

  • Ready Callback: Sensors_TemperatureReadyCb() - Called when temperature measurement is complete

Usage:#

  • One-shot measurement: NBU requests with interval = 0

  • Periodic measurement: NBU requests with interval > 0 (in milliseconds)

  • The periodic measurement continues until a new request changes the interval or stops it

Temperature Filtering and NBU Communication#

Modified Moving Average Filter#

On wireless_mcu platforms, temperature readings are processed through a Modified Moving Average (MMA) filter to reduce noise and prevent unnecessary NBU notifications. This filter helps to:

  • Limit XTAL32M calibration changes: Prevents excessive calibration adjustments that could degrade RF performances

  • Optimize power consumption: Reduces NBU wake-up events by limiting notifications to significant temperature changes

  • Reduce noise: Smooths out temperature reading fluctuations for more stable system behavior

The XTAL32M calibration process uses a LUT (Look-Up Table) that contains pre-characterized calibration values mapping temperature ranges to optimal XTAL32M frequency adjustments, enabling precise crystal oscillator tuning based on thermal conditions.

The LUT is registered using PLATFORM_RegisterXtal32MTempCompLut() and this is currently done in examples/_common/project_segments/wireless/wireless_mcu/app_common/hardware_init.c and requires gBoardUseXtal32MTempComp to be enabled.

Configuration: Filter size is controlled by PLATFORM_TEMPERATURE_FILTER_SIZE (default: 4 samples)

NBU Temperature Threshold#

Temperature values are only sent to the NBU when they exceed a configurable threshold:

Threshold is Controlled by PLATFORM_TEMP_SENT_NBU_THRESHOLD (default: 10 tenths of degrees Celsius = 1°C)

Temperature Processing Flow:#

  1. Raw Measurement: ADC interrupt captures temperature reading

  2. Sensors Module Informed Sensors referesh the temperature value

  3. Filtering: Raw value is processed through MMA filter

  4. Threshold Check: Filtered value is compared against last sent value ± threshold

  5. NBU Communication: If threshold is exceeded:

    • XTAL32M calibration is performed (if LUT is available)

    • Temperature value is sent to NBU

    • Last sent value is updated

Temperature Request
           ↓
ADC Interrupt - Measurement is ready
           ↓
Raw Temperature Reading
           ↓
Sensors Module Informed - Temperature refresh
           ↓
MMA Filter Processing
           ↓
Threshold Check: |filtered - last_sent| > threshold?
      ↓                    ↓
    YES                   NO
      ↓                    
LUT Available?
   ↓        ↓
 YES       NO
   ↓        ↓
XTAL32M     ↓
Calibration ↓
   ↓        ↓
   └────────┘
      ↓
Send Temperature to NBU
      ↓
Update Last Value Sent to NBU

Platform Configuration Macros:#

// Temperature filter size (number of samples for averaging)
#define PLATFORM_TEMPERATURE_FILTER_SIZE 4U

// Threshold for sending temperature to NBU (in tenths of degrees Celsius)
#define PLATFORM_TEMP_SENT_NBU_THRESHOLD 10  // 1°C

API Usage Examples#

Manual Temperature Measurement#

int32_t temperature1, temperature2;
SENSORS_TriggerTemperatureMeasurement();
...
temperature1 = (SENSORS_RefreshTemperatureValue())/10;
temperature2 = (SENSORS_GetTemperature())/10;

In this case temperature1 is equal to temperature2, both are in degree celsius.

Battery Level Measurement#

uint8_t batteryLevel;
SENSORS_TriggerBatteryMeasurement();
...
batteryLevel = SENSORS_RefreshBatteryLevel();
// batteryLevel is now in percentage (0-100%)

Handling Concurrent Requests#

// First request - will be accepted
SENSORS_TriggerTemperatureMeasurement();

// Second request while first is ongoing - will be dropped silently
SENSORS_TriggerBatteryMeasurement();  // This will be ignored

// Wait for first measurement to complete
int32_t temp = SENSORS_RefreshTemperatureValue();

// Now battery measurement can be triggered
SENSORS_TriggerBatteryMeasurement();  // This will be accepted

Low Power Optimization - Wake-up Temperature Measurement#

// In low power exit callback (interrupts masked, scheduler disabled)
/* Trig temperature measurement on wake-up.
 * If a temperature change is detected,
 * the new value will be sent to the NBU for appropriate XTAL32M trimming.
 * During channel sounding measurements, this temperature is also used for RTT compensation.
 * Since this function runs with interrupts masked and the scheduler disabled,
 * the unsafe variant must be used to avoid mutex acquisition.
 */
SENSORS_TriggerTemperatureMeasurementUnsafe();

This approach optimizes power consumption and provides additional benefits:

  • XTAL32M Trimming: Temperature changes are sent to NBU for crystal oscillator calibration only if they exceed the configured threshold after filtering

  • RTT Compensation: This temperature data is used by the NBU for RTT compensation during channel sounding measurements

  • Safe Execution: Uses the unsafe variant to avoid mutex acquisition in interrupt context with scheduler disabled In case of periodic measurement:

  • Power Optimization: Triggers temperature measurements when the system is already awake, avoiding dedicated timer wake-ups

  • Timer Reset: Resets the periodic measurement timer to prevent unnecessary wake-ups

Note: This optimization is implemented by default in wireless platform examples when gAppUseSensors_d is enabled. The temperature measurement is automatically triggered in the low power exit callback (BOARD_ExitLowPowerCb()) in examples/_common/project_segments/wireless/wireless_mcu/board_lp.c.

Constant macro definitions#

Name :

#define VALUE_NOT_AVAILABLE_8 0xFFu
#define VALUE_NOT_AVAILABLE_32 0xFFFFFFFFu

Description :

Defines the error value that can be compared to the value obtain on the ADC.