BDB_eOutOfBandCommissionGetDataEncrypted#
BDB_teStatus BDB_eOutOfBandCommissionGetDataEncrypted(
BDB_tsOobWriteDataToAuthenticate *psSrcCredentials,
uint8 *pu8ReturnAuthData,
uint16 *puSize);
Description#
This function is used to obtain locally stored commissioning data, including the network key which returns encrypted. Authentication data (including an install code) must be provided which is used to encrypt the network key.
The obtained data is received as a byte stream - the size of the byte stream is also returned. The byte stream contains the following data:
IEEE/MAC address of the local node as
u64address(8 bytes)Network key encrypted with the data passed via psSrcCredentials (16 bytes)
MIC value generated to validate encryption (4 bytes)
Key sequence number of active network key (1 byte)
Active channel number (1 byte)
PAN ID (2 bytes)
Extended PAN ID (8 bytes)
The encrypted network key and other obtained data are then sent by out-of-band means to the other device involved in the commissioning. The receiving device may decrypt the key using the BDB_bOutOfBandCommissionGetKey() function.
A similar set of data without encryption of the network key is obtained using the function BDB_u8OutOfBandCommissionStartDevice().
For an overview of out-of-band commissioning, refer to Out-Of-Band Commissioning.
Parameters#
psSrcCredentials: Pointer to a structure containing authentication data to be used to encrypt the network key (see BDB_tsOobWriteDataToAuthenticate).
pu8ReturnAuthData: Pointer to the start of the returned byte stream containing the obtained data.
puSize: Pointer to a location to receive the size of the obtained byte stream.
Returns#
None
Parent topic:Functions