eSE_PriceCreate
teSE_PriceStatus eSE_PriceCreate(
bool_t bIsServer,
uint8 u8NumberOfRecordEntries,
uint8 *pu8AttributeControlBits,
uint8 *pau8RateLabel,
tsZCL_ClusterInstance *psClusterInstance,
tsZCL_ClusterDefinition *psClusterDefinition,
tsSE_PriceCustomDataStructure
*psCustomDataStructure,
tsSE_PricePublishPriceRecord
*psPublishPriceRecord,
void *pvEndPointSharedStructPtr);
Description
This function creates an instance of the Price cluster on an endpoint. The cluster instance is created on the endpoint which is associated with the supplied tsZCL_ClusterInstance
structure and can act as a server or a client, as specified.
The function should only be called when setting up a custom endpoint containing one or more selected clusters (rather than the whole set of clusters supported by a standard ZigBee device). This function will create a Price cluster instance on the endpoint, but instances of other clusters may also be created on the same endpoint by calling their corresponding creation functions. For more details of creating cluster instances on custom endpoints, refer to Appendix D.
Note: This function must not be called for an endpoint on which a standard ZigBee device (e.g. IPD) will be used. In this case, the device and its supported clusters must be registered on the endpoint using the relevant device registration function from those described in the ZigBee Devices User Guide (JNUG3131)
When used, this function must be the first Price cluster function called in the application, and must be called after the stack has been started and after the ZCL has been initialized.
The function requires an array to be declared for internal use, which contains one element (of type uint8) for each attribute of the cluster. The array length should therefore equate be the total number of attributes supported by the Price cluster, which can be obtained by using the macro PRICE_NUM_OF_ATTRIBUTES.
The array declaration should be as follows:
uint8 au8AppPriceClusterAttributeControlBits[PRICE_NUM_OF_ATTRIBUTES];
The function initializes the array elements to zero.
The function also requires an array of price labels to be declared, in which each array element is a label (string) for each price in the price list. The required declarations are different for a cluster server and client, as follows:
uint8 au8RateLabel[SE_PRICE_NUMBER_OF_CLIENT_PRICE_RECORD_ENTRIES][SE_PRICE_CLIENT_MAX_STRING_LENGTH];
uint8 au8RateLabel[SE_PRICE_NUMBER_OF_CLIENT_PRICE_RECORD_ENTRIES][SE_PRICE_CLIENT_MAX_STRING_LENGTH];
Parameters
bIsServer Type of cluster instance (server or client) to be created:
TRUE - server
FALSE - client
u8NumberOfRecordEntries Number of prices that can be stored in the price list, one of:
SE_PRICE_NUMBER_OF_SERVER_PRICE_RECORD_ENTRIES
SE_PRICE_NUMBER_OF_CLIENT_PRICE_RECORD_ENTRIES
pu8AttributeControlBits Pointer to an array of uint8 values, with one element for each attribute in the cluster (see above).
pau8RateLabel Pointer to an array of price labels (strings), with one element for each price in the price list (see above).
psClusterInstance Pointer to structure containing information about the cluster instance to be created (see Section 6.1.16). This structure is updated by the function by initialising individual structure fields.
psClusterDefinition Pointer to structure indicating the type of cluster to be created (see Section 6.1.2). In this case, this structure must contain the details of the Price cluster. This parameter can refer to a pre-filled structure called
sCLD_Price
which is provided in the Price.h file.psCustomDataStructure Pointer to structure which contains custom data for the Price cluster. This structure is used for internal data storage. No knowledge of the fields of this structure is required
pvEndPointSharedStructPtr Pointer to the shared structure used for attribute storage. This parameter should be the address of the structure of type
tsCLD_Price
which defines the attributes of Price cluster. The function initializes the attributes with default values.
Returns
E_ZCL_SUCCESS
E_ZCL_FAIL
E_ZCL_ERR_PARAMETER_NULL
E_ZCL_ERR_INVALID_VALUE
Parent topic:Functions