MCUXpresso SDK Documentation

tsZCL_ClusterDefinition

tsZCL_ClusterDefinition#

This structure defines a cluster used on a device:

typedef struct
{
    uint16                      u16ClusterEnum;
    bool_t                      bIsManufacturerSpecificCluster;
    uint8                       u8ClusterControlFlags;
    uint16                      u16NumberOfAttributes;
    tsZCL_AttributeDefinition  *psAttributeDefinition;
    tsZCL_SceneExtensionTable  *psSceneExtensionTable;
#ifdef ZCL_COMMAND_DISCOVERY_SUPPORTED    
    uint8                       u8NumberOfCommands;
    tsZCL_CommandDefinition    *psCommandDefinition;
#endif 
}  tsZCL_ClusterDefinition;

Where:

  • u16ClusterEnum is the Cluster ID.

  • bIsManufacturerSpecificCluster indicates whether the cluster is specific to a manufacturer (proprietary):

    • TRUE - proprietary cluster

    • FALSE - ZigBee cluster


u8ClusterControlFlags is a bitmap containing control bits in two parts, as follows:

Bits

Description

Values

0 - 3

Type of security

Indicates the type of security key used via one of the following teZCL_ZCLSendSecurity enumerations (see Section 7.1.6):

Bits

Description

Values

0 - 3

Type of security

Indicates the type of security key used via one of the following teZCL_ZCLSend Security enumerations (see Section 7.1.6):   E_ZCL_SECURITY_NETWORK, E_ZCL_SECURITY_APPLINK
•  E_ZCL_SECURITY_TEMP_APPLINK
(this option is for internal use only)

4 - 7

Cluster mirror

Used internally to indicate whether the cluster is mirrored, as follows:
•  0000b - Not mirrored,1000b - Mirrored, All other values are reserved

  • u16NumberOfAttributes indicates the number of attributes in the cluster.

  • psAttributeDefinition is a pointer to an array of attribute definition structures - see Section 6.1.3.

  • psSceneExtensionTable is a pointer to a structure containing a Scene Extension table - see Section 6.1.20.

  • The following optional pair of fields are related to the Command Discovery feature (see Section 2.9):

    • u8NumberOfCommands is the number of supported commands in the Command Definition table (see below).

    • psCommandDefinition is a pointer to a Command Definition table which contains a list of the commands supported by the cluster - each entry of the table contains the details of a supported command in a tsZCL_CommandDefinition structure (see Section 6.1.19).

Parent topic:General Structures