Secure Provisioning Tool 26.09.1

Generic workflows

Generic workflows#

This section provides information on workflow for some typical use cases. These chapters are not specific for any processor.

Debug authentication workflow#

This section describes the process of opening the debug port using Debug Authentication Protocol (DAP) as a mechanism to authenticate the debugger (an external entity) for the field technician, which has the credentials approved by the product manufacturer (OEM) before granting the debug access to the device. For Debug Authentication (DA) to work, processor-specific fuses or PFR fields must be set. For more information see the device user manual, chapter Debug subsystems.

_images/Debug_Authentification_protocol_usage_example.svg

Fig. 74 Debug Authentification protocol usage example#

This section applies to processors with Debug Mailbox. There are also processors (such as MCXE31x) where debug authentication can be done with:

  • plain password - this is not supported in the SEC tool and the debug probe CLI should be used;

  • challenge/response authentication - this is described in processor specific workflow.

To open the debug port using Debug Mailbox DAP, cooperation is required between the field technician requesting access and the OEM owning the ROT keys and granting access. The typical procedure is:

Field Technician

  1. To get the key type and ROT length, contact the OEM. OEM decides whether to use the generated certificate for any device with the same ROT keys or just one by specifying the UUID.

  2. In the SEC Tool, create a workspace for the target device and open the Debug Authentication tool using main menu > Tools > Debug Authentication. Alternatively, it is also possible to use the actions on the “PKI Management” view.

  3. Click the Create debug certificate request… button. Generate a debug authentication (DA) key if one does not exist yet. Ensure both the key type and length of the DA key match those of the corresponding ROT key.

  4. Optionally, specify an UUID to limit the use of the debug certificate. UUID can be read from a device via UART or USB if the processor is in ISP mode and in the development life cycle or via debug probe. For processors in an advanced life cycle, the debug probe still can be used. UUID verification in the chip is provided if CHECK_UUID field is set in the SOCU fuse/PFR field.

  5. In the Note field, you can optionally specify a comment or reason for the OEM. This note is visible only in the communication; it is not stored in the certificate.

  6. Send the certificate request to OEM

  7. After the certificate from OEM is received, click the Open debug port… button. The connected probes are detected upon the dialog display. The list of detected probes can be updated by clicking the Find probes button. Select one of the detected probes. The authentication beacon is an optional parameter and it is independent of the credential beacon provided by the OEM. It is not interpreted by the debug authentication protocol, it is passed to the debugged application.

  8. For devices with a dual key schema, it is necessary to provide the path to the manifest file, which contains information about the public keys and indicates which key was used for signing. The preferred approach is to provide the path to the certificate ZIP file, from which the manifest path will be prefilled and the correct dir structure with public keys will be created.

  9. When the dialog is confirmed, a script is generated in workspace\debug_auth\open_debug_port.bat/sh and is executed. The dialog is closed if no error is reported by the script (the operation is successful). In case of failure, refer to section Debug authentication for details on how to enable debug authentication.

_images/Dialog_for_opening_debug_port.png

Fig. 75 Dialog for opening debug port#

Note: the debug authentication can be done also on command line using securep debug-auth command.

OEM Developer

After receiving the request, click the Generate debug certificate… button.

The certificate is by default generated into <workspace>/debug_authfolder, debug_auth_cert.dc. A *.zip archive with the same name is created, it contains the certificate and the .txt file note from OEM. For devices that support the dual key schema, the created ZIP file also contains a manifest with additional information for DA configuration and public keys. The note that is passed from field technician to OEM is displayed in the note field (see Figure “Generation of debug certificate from certificate request”).

  • SoC - mask value of DCFG_CC_SOCU controlling which debug domains are accessed via the authentication protocol

  • Vendor usage - field that can be used to define a vendor-specific debug policy. The use case can be Debug Credential (DC) certificate revocations, the department identifier, or the model identifier.

  • Credential beacon - a value that is not interpreted by DAP, it is passed to the application. The value is independent of the authentication beacon that will be provided by the field technician when the port is opened.

  • Note - text field where OEM can describe comments about reasons to generate the certificate

  • Sign with ROT key - sign the certificate with one of the ROT keys that were used to secure the device.

_images/Generation_of_debug_certificate_from_certificate_request.png

Fig. 76 Generation of debug certificate from certificate request#

Example of access rights to debug domains#

Examples are intended for testing purposes. Before the final usage, the setting should be revisited and modified to fulfill security requirements. In all examples below, ISP is enabled and UUID check is disabled. For some processors, UUID check must be set to enable the read of UUID by a debug probe.

Table 36. KW45xx/K32W1xx and MCX W71x#

Fuse

Everything disabled

Everything enabled

Controlled by DA

DCFG_CC_SOCU_L1, DCFG_CC_SOCU_L2

0x000000FF

0x0000FFFF

0x00004040

DBG_AUTH_DIS

0x0

0x0

0x0

Table 37. KW47xx and MCX W72x#

Fuse

Everything disabled

Everything enabled

Controlled by DA

DCFG_CC_SOCU_L1, DCFG_CC_SOCU_L2

0x000001FF

0x0003FFFF

0x00008040

DBG_AUTH_DIS

0x0

0x0

0x0

Table 38. LPC55S0x/1x, MCXW236 and NHS52S04#

PFR field

Everything disabled

Everything enabled

Controlled by DA

DCFG_CC_SOCU_NS_PIN, DCFG_CC_SOCU_PIN

0xFF2000DF

0xFF2000DF

0xFFBF0040

DCFG_CC_SOCU_NS_DFLT, DCFG_CC_SOCU_DFLT

0xFFFF0000

0xFF2000DF

0xFFBF0040

Table 39. LPC55S2x#

PFR field

Everything disabled

Everything enabled

Controlled by DA

DCFG_CC_SOCU_NS_PIN, DCFG_CC_SOCU_PIN

0xFF2000DF

0xFF2C00D3

0xFFBF0040

DCFG_CC_SOCU_NS_DFLT, DCFG_CC_SOCU_DFLT

0xFFFF0000

0xFF2C00D3

0xFFBF0040

Table 40. LPC55S3x#

PFR field

Everything disabled

Everything enabled*

Controlled by DA

DCFG_CC_SOCU_NS_PIN, DCFG_CC_SOCU_PIN

0xFE3001CF

0xFE3001CF

0xFFFF0000

DCFG_CC_SOCU_NS_DFLT, DCFG_CC_SOCU_DFLT

0xFFBF0040

0xFE3001CF

0xFFFF0000

Note: For debugging, authentication is still required but the domain cannot be disabled by the SoC mask in the DAC.

Table 41. LPC55S6x#

PFR field

Everything disabled

Everything enabled

Controlled by DA

DCFG_CC_SOCU_NS_PIN, DCFG_CC_SOCU_PIN

0xFD0002FF

0xFD0002FF

0xFFBF0040

DCFG_CC_SOCU_NS_DFLT, DCFG_CC_SOCU_DFLT

0xFFBF0040

0xFD0002FF

0xFFBF0040

Table 42. MCX Nx4x, MCX N23x and MCX N55xS#

PFR field

Everything disabled

Everything enabled*

Controlled by DA

DCFG_CC_SOCU_NS_PIN, DCFG_CC_SOCU_PIN

0xF81007EF

0xF81007EF

0xFFBF0040

DCFG_CC_SOCU_NS_DFLT, DCFG_CC_SOCU_DFLT

0xFFBF0040

0xF81007EF

0xFFBF0040

Note: For debugging, authentication is still required but the domain cannot be disabled by the SoC mask in the DAC.

Table 43. RT5xx/6xx#

Fuse

Everything disabled

Everything enabled

Controlled by DA

DCFG_CC_SOCU, DCFG_CC_SOCU_NS

0x80FF408D

0x80FFFF20

0x00404088

DCFG_CC_SOCU_AP

0x7F00BF72

0x7F0000DF

0xFFBFBF77

Table 44. RW61x#

Fuse

Everything disabled

Everything enabled*

Controlled by DA

DCFG_CC_SOCU, DCFG_CC_SOCU_NS

0x3FFA007E

0x3FFFFF14

0x1002000F

DCFG_CC_SOCU_AP

0xC005FF81

0xC00000EB

0xEFFDFFF0

Note: For debugging, authentication is still required but the domain cannot be disabled by the SoC mask in the DAC.

RT118x does not have any fuse to control the debugging rights. Debugging behavior depends on the life cycle state:

  • OEM_OPEN: All debug is allowed.

  • OEM_CLOSE: All debug is disabled by default but can be re-enabled using DAC.

  • OEM_LOCKED: All debug is disabled and cannot be re-enabled.

Debug authentication application notes#

See application note: MCXN Debug Authentication

Signature provider workflow#

This section describes the process of setting up a signature provider and building an image signed by the signature provider. Examples of signature provider servers are available in <install_folder>/sample_data/signature_provider_examples. There are several servers supporting signing with RSA, ECC, and RSA/ECC using a certificate authority (CA). These examples demonstrate a full implementation of the API; however, in the real world, it is expected that the implementation will be changed by communication with an HW HSM module or custom HTTPS communication with another server. Examples of the server can be used to test the tool behavior when using the signature provider. Each server has example private keys and prepared public key response for the public_keys_certs endpoint. These keys should not be used in final products.

Table 45. Key types supported in the server examples#

Server example

Private keys

Public keys tree

ca_rsa_ecc_server

CA-4xSRK-4xCSF-4xIMG ECC-p256
CA-4xSRK-4xCSF-4xIMG RSA-2048

hex of certs

ecc_server

4xROT-4xIMG ECC-p256

hex of public keys

rsa_server

4xROT-4xIMG RSA-2048

hex of public keys

rt118x_ecc_rsa_server

4xSRK ECC-p256
4xSRK RSA-2048

hex of public keys

The figure below displays variants of signature provider, the SEC Tool sends requests to a Custom signature provider HTTP server. This server should pass the request to one of the secure solutions and then pass the response back to the SEC Tool. Prepared examples implement only the Custom signature provider HTTP server. The example server is doing the operation that should be done by an HSM or external signature provider. It is up to the user to implement a complete solution.

_images/Expected_structure_of_signature_provider.svg

Fig. 77 Expected structure of signature provider#

Run the server#

Ensure that python 3.12 or higher is installed. Open the directory with the server implementation(click the Sample server implementations link in signature provider dlg), specify the SPSDK package version in requirements.txt (use the same version as shown in Menu bar > Help > About), and run the following commands:

# ensure, venv is installed
pip install virtualenv
# create virtual environment into .venv subfolder
python -m venv ".venv"
# activate it
.venv\Scripts\activate
# install all required packages into venv
pip install -r requirements.txt
# start the server
python server.py

The server logs every action, so it is possible to review what actions were executed.

Set up in the SEC Tool#

To use the signature provider example with the SEC Tool, follow these steps:

  1. Create/use workspace for the processor.

  2. Select the check-box Use sign. provider on the PKI tab. If there are keys in the workspace, they are moved to a back-up subfolder in the workspace.

  3. Open the signature provider dialog by clicking Configure… next to the check-box from step 2.

  4. Review the default parameters of your signature provider. If using the signature provider server from resources\signature_provider_examples, the default settings work.

  5. Select the prehash option in the parameters table. When prehash is enabled, only a hash of the data is sent to the server for signing. Not all processors support all hash options. For example, processors with MBI can use only hash algorithms whose output length matches the length of the signing keys. See the reference manual for processor-specific details.

  6. Click the Test connection button to verify if the server is configured properly.

  7. There are two options to Import public keys:

    • In the same dialog, click the Import public keys button to import public keys from the server; this is a recommended way, however it can be used only if the server implements optional API public_keys_certs.

    • If the Import public keys command is not supported, the alternative way is to use Import keys from the PKI management tab. Make sure that public keys match private keys that are used on the signature provider site (copy the keys to the folder with the signature provider example).

  8. On the Build tab, select the key as normally, now the config files for SB, MBI, and certification block will be using the signature provider configuration.

  9. Now, the signature provider is configured. It is possible to build a signed image.

Signature provider and debug authentication#

The SEC Tool supports signing of the DA certificate by the signature provider. The field technician flow of the DA key generation is the same as without the signature provider; the debug key pair generation is supported only locally. The only difference is that in the DAC generation on the OEM site, the signature provider is used for signing. This is transparent to the user as the public key is selected from the workspace keys. The only difference is in the generated configuration file, where the sign_provider field is set according to the signature provider setting.

Script hooks workflow#

Script hooks are executed before or during build, write, and manufacturing script execution. Script hooks enable script customization outside the generated scripts. Hook scripts are located in the “hooks” subfolder and the new workspace contains the examples for the selected processor. Script hooks are not generated by the tool; they are expected to be fully under user control. If the hook script does not exist, it can be created with a single click in the GUI.

Build script hooks#

  1. Pre-build hook: pre_build_<os-name>.bat/sh is executed before the build script. This script can be generated to sign the MCUboot application image. This script does not have any argument and it is called only from the GUI before the build script is executed.

  2. Build context hook: build_context_<os-name>.bat/sh is called at the beginning of the build script and allows users to add or modify the environment variables. This hook is called without arguments.

  3. Build hook: the build_.bat/sh script is executed after each main step in the build script. This script is called from the build script and the name of the previous step is passed as an argument. All the supported steps are handled in the generated examples. If a hook step call fails, the build script execution stops and exits with an error.

Write script hooks#

  1. Write the context hook: the write_context_<os-name>.bat/sh script is called at the beginning of the write script and allows users to add or modify the environment variables. This hook is called without arguments.

  2. Write the hook: the write_<os-name>.bat/sh script is executed after every main step in the write script. The script is called from the write script and the name of the previous step is passed as an argument. All the supported steps are handled in the generated example. If a hook step call fails, the write script execution stops and exits with an error.

Manufacturing hooks#

Manufacturing hook: manufacturing_<os-name>.bat/sh is called at the beginning and end of the manufacturing process before the first task is started and after the last task is finished. If manufacturing hook execution for step started fails, planned manufacturing steps are not executed. The call for step finished has an additional argument status that can have two values ok or fail that denote the execution status of the manufacturing process: ok if all tasks were finished successfully, fail otherwise.

Typical usage#

Here are a few examples how the hook scripts can be used to customize the build, write, or manufacturing script without the modification of the script generated from the SEC Tool:

  • Update the input source file(s) for the build.

  • Fix the problem in the write script or apply an additional action that updates the previous action.

  • Synchronize the manufacturing operation with the assembly line.

Zephyr#

This chapter describes the steps to successfully boot up the device Zephyr-based projects. It describes the VS Code setup, creation of the bootable image, connecting your device, setting up your boot preferences, and writing the image into the selected boot memory. Common steps are described first, followed by device family-specific content. It is assumed that the image is executed on an NXP evaluation board.

This chapter addresses image preparation for the VS Code IDE.

** Note: **: Debug build configuration is used unless specified differently. For Release build configuration, the steps are the same.

More information about Zephyr, VS Code, and MCboot can be found at:

Common steps#

Prerequisites#

Option if VS Code is not installed yet:

  • Use the MCUXpresso Installer to set up all required dependencies, including VS Code; make sure that you select the “Zephyr Developer” option.

Option if VS Code is already installed:

  • Install the “MCUXpresso for VS Code” extension for VS Code: https://marketplace.visualstudio.com/items?itemName=NXPSemiconductors.mcuxpresso

  • Use the MCUXpresso Installer to set up all required dependencies; make sure that you select the “Zephyr Developer” option.

Import Zephyr repository#

  1. Open the MCUXpresso for VS Code extension.

  2. From the Quick Start panel, select “Import Repository” (A remote repository was used for this workflow, although other options are also supported).

  3. Select the latest Zephyr revision (v4.3.0 was used for the following workflows) and specify the target folder.

  4. Click the Import button.

Standalone Zephyr application#

This chapter describes the steps to successfully boot up the device Zephyr-based project without a secondary bootloader.

Project creation#

  1. In VS Code, from the Quick Start panel, select “Import Example from Repository”.

  2. Select the cloned repository from the previous step.

  3. Select your board.

  4. Select the “zephyr/samples/basic/blinky” template.

  5. Select “App type” as the “Freestanding Application”.

  6. Fill in the project name, location path.

  7. Select Zephyr-SDK - Default Zephyr SDK.

  8. Click the Import button.

  9. Build an application.

Setting up Secure Provisioning Tool#

  1. Start Secure Provisioning Tool:

  • Windows: Double-click the desktop shortcut, or use the Windows Start menu to locate the tool.

  • MacOS: Click the shortcut in the Dock, or use the Launchpad to locate the tool.

  • Linux: Click the shortcut in the Launcher, or use the Dash to locate the tool.

  1. Create a workspace by selecting File > New workspace … from the menu bar. Select the path to the new workspace. Then select the target processor and click Create.

  2. Connect the device to the host through USB, UART, SPI, or I2C.

  3. Confirm that the connection is working by selecting Target > Connection … from the menu bar and clicking the Test button. Tweak if necessary.

  4. Configure the Source Image as <project-path>/debug/zephyr/zephyr.elf or <project-path>/debug/zephyr/zephyr.bin.

  5. If a pop-up dialog detecting DCD/FCB appears, confirm the defaults.

  6. Check if the target memory is correct based on your board and project.

  7. Switch the board to ISP mode.

  8. Build and Write application to the device.

  9. Switch the board to run boot from the selected target memory, reset.

MCUBoot Zephyr application#

This chapter describes the steps to successfully boot up the device Zephyr-based project with the MCUboot secondary bootloader. The MCUboot is part of the described example project, so only one project is imported. This chapter does not cover neither replacing the signing key nor signing by the SEC tool as it requires extra changes in the VS Code project and Zephyr does signing of the application automatically.

Project Creation#

  1. In VS Code, from the Quick Start panel, select “Import Example from Repository”.

  2. Select the cloned repository from the previous step.

  3. Select your board.

  4. Select the “bootloader/mcuboot/samples/zephyr/hello-world” template.

  5. Select “App type” as the “Freestanding Application”.

  6. Fill in the project name, location path.

  7. Select the Zephyr-SDK - Default Zephyr SDK.

  8. Click the Import button.

  9. Build the application.

During the build several MCUboot actions are executed:

  1. Exporting the public portion of the signing key into the C file (autogen-pubkey.c).

  2. The MCUboot application is built into debug/mcuboot/zephyr/zephyr.bin.

  3. The application itself is built into debug/boot-zephyr-hello-world/zephyr/zephyr.bin.

  4. The application is signed with the private key into a new file debug/boot-zephyr-hello-world/zephyr/zephyr.signed.bin.

It is necessary to get information on which address the signed application is programmed into the memory. In the debug/boot-zephyr-hello-world/zephyr/zephyr_final.map file in the “Memory Configuration” section, the “FLASH” row and “Origin” column contain this information. For example, for MIMXRT1060-EVKC it is 0x60020000.

Setting up Secure Provisioning Tool#

  1. Start Secure Provisioning Tool:

  • Windows: Double-click the desktop shortcut, or use the Windows Start menu to locate the tool.

  • MacOS: Click the shortcut in the Dock, or use the Launchpad to locate the tool.

  • Linux: Click the shortcut in the Launcher, or use the Dash to locate the tool.

  1. Create a workspace by selecting File > New workspace … from the menu bar. Select the path to the new workspace. Then select the target processor and click Create.

  2. Connect the device to the host through USB, UART, SPI, or I2C.

  3. Confirm that the connection is working by selecting Target > Connection … from the menu bar and clicking the Test button. Tweak if necessary.

  4. Configure the Source Image as <project-path>/debug/mcuboot/zephyr/zephyr.elf or <project-path>/debug/mcuboot/zephyr/zephyr.bin (the MCUboot).

  5. If a pop-up dialog detecting DCD/FCB appears, confirm the defaults.

  6. Check if the target memory is correct based on your board and project.

  7. Click the Additional images button, configure for example, Image 1 to zephyr.signed.bin, set the “Boot mem. addr” obtained from the zephyr_final.map file. Confirm the dialog.

  8. Switch the board to ISP mode.

  9. Build and Write application to the device.

  10. Switch the board to run boot from the selected target memory, reset.

Zephyr examples with MCUboot in different memory#

Not every Zephyr example project can be used as it is. Additional workflow or changes in the project are required. For example, in older Zephyr for MCX N devices, the QSPI examples require a (MCUBoot) bootloader in the internal flash by default. The default start address is not usable for a bootable image creation without the bootloader. For details, see the Zephyr documentation for the given board. Either the bootloader in the internal flash has to be used or the start address must be changed. For the mentioned MCX N devices, the start address can be changed in the build/zephyr/.config file:

CONFIG_FLASH_BASE_ADDRESS=0x90000000

has to be changed to

CONFIG_FLASH_BASE_ADDRESS=0x90001000

Disabling MCUboot in Zephyr examples#

If MCUboot is not required but is enabled in the example, it can be disabled by modifying the following files:

  • prj.conf:

    CONFIG_BOOTLOADER_MCUBOOT=n
    
  • sysbuild.conf:

    SB_CONFIG_BOOTLOADER_MCUBOOT=n
    

Manufacturing workflow#

For the manufacturing operations, the tool offers a simplified user interface focused on the manufacturing only.

Create manufacturing package#

OEM can create a manufacturing package (*.zip) that can be used to transfer files to the factory. The manufacturing package can be created:

  • On the Write image view - for provisioning using the current write script

  • In the SB editor - to apply commands specified in the SB file

_images/Create_Manufacturing_Package_dialog.png

Fig. 78 Create Manufacturing Package dialog#

The Create Manufacturing Package dialog allows the user to:

  • Check package parameters overview.

  • Review files included in the package.

  • Check the write script arguments, the arguments are in the same format as they are used in Manufacturing Tool.

  • Select the output manufacturing package file path.

  • Set the password for the ZIP file. The AES algorithm is used to encrypt files in the ZIP file; however, the file metadata (like file names and file sizes) are not encrypted.

  • For the EdgeLock 2GO provisioning, it is possible to optionally specify the API key in the manufacturing package, but it can be specified later during manufacturing

Performance optimization#

It is supposed that the provisioning/write script will be executed several times to address different development issues, so the script is designed primary for this use case and may contain some parts that are not necessary in manufacturing when the provisioning is applied to an empty processor. Here are some tips to improve manufacturing performance by manually modifying the generated script:

  • It might not be needed to erase boot memory. If the processor is new, the flash is already erased.

  • It might not be needed to detect if the chip is already secured; this part in the write script allows updating application for secured processors (for chips where it is supported)

  • A longer sequence of blhost operations might not be optimal, because the blhost initialization time is not insignificant. It might be better to move the operations into the SB file (see SB editor) or use blhost batch command (see SPSDK documentation for details).

  • If the processor is reset during manufacturing, there is a delay time until it boots and the OS driver reconnects. By default, it is 3 seconds. The time can be adjusted in preferences.

Manufacturing operations#

On the manufacturing site, the manufacturing package can be imported using main menu > File > Import Manufacturing Package…. During import, the files from the package are extracted into the new workspace - called manufacturing workspace. For more information about importing the package, see Import workspace from the ZIP.

Once the workspace is created (or reopened), the Manufacturing Tool (for details, see Manufacturing Tool ) is displayed, and the rest of the tool functionality is not available. If the Manufacturing Tool is closed, the whole tool operation is finished. If you restart the tool, it offers to continue manufacturing, or to select another workspace:

_images/Confirmation_to_reopen_manufacturing.png

Fig. 79 Confirmation to reopen manufacturing#

If the manufacturing package contains a write script, check if the SPT_INSTALL_BIN environment variable in the script points to the installation directory on the computer. If not, it is recommended to set the environment variable globally or update the write script manually.

For serial connection: Adjust the baud rate, the default value is 115200; however, for several processors, baud rates up to 1000000 were successfully tested.

Steps in the manufacturing production#

  1. Connect one or more processors via USB or serial line or I2C or SPI and click the Autodetect button to detect the connected devices. In case the tool detects devices that should not be affected by the manufacturing, such as serial ports used by other devices, disable them. Then click Test connection below to check the connection with all enabled processors and ensure the test passes.

  2. To start the trust provisioning operation, click the Start button. Wait until all operations are finished.

  3. If any problem is reported, click to the status cell to show the log and fix the problem.

  4. Continue with step 1

The number of successfully provisioned devices is displayed on the bottom of the Manufacturing Tool window, but it is not 100% reliable.

Manufacturing logs#

Manufacturing logs are stored in the manufacturing workspace, in the subdirectory logs/YYYY-MM-DD/. The log file name is manufacturing_log_YYYY-MM-DD_hh-mm-ss_#.log, where # represents index of the manufacturing task being executed in parallel. It is possible to export them using the Export logs button from the manufacturing window. The export allows to select one day (a date) or all logs and exports the selected logs into the ZIP file.

MCUboot workflow#

MCUboot is an open source secure bootloader for 32-bit microcontrollers. For details, see MCUboot Documentation. It has been ported to many NXP processors, and you can find it supported in the MCUXpresso SDK. For details, see boards\<board>\ota_examples\mcuboot*.

For most of the processors, the SEC Tool contains a default configuration compatible with project examples provided in the MCUXpresso SDK. Therefore, there is a “sample application” built from MCUXpresso SDK for the EVK/FRDM board and the default imgtool parameters match MCUXpresso SDK.

For the rest of the processors, the support for MCUboot was not tested; however, it can still be configured in the SEC Tool.

Steps to start MCUboot for NXP board via New Workspace#

  1. Open the New Workspace dialog and select the processor.

  2. Connect the board via UART, ensure that the processor boot is in ISP mode. It is possible to use other connections, the UART is used because the mcuboot application is built with the debug console and prints the status that can be verified using the terminal.

  3. Select the MCUboot bootloader image, and the corresponding sample application for the selected processor (including both the bootloader and executable image) will be automatically chosen. If no image is selected, it indicates that a sample application is not available for the selected processor. In such cases, refer to the manual configuration instructions below

  4. Click OK to create new workspace. If the tool offers to use FCB (Flash Configuration Block) from the source image, select the checkbox to use it, because on some processors, MCUboot requires certain flash configuration.

  5. The MCUboot Sign Image dialog will open with all required options preselected, so it is possible to save the options and sign the image.

  6. Build and write the bootable image into the processor. Note: To verify everything works correctly, refer to step 9. of the manual configuration below.

Steps to start MCUboot with such a processor manually#

  1. Create a new workspace for the selected processor.

  2. Connect the board via UART, ensure that the processor boot is in ISP mode, and check the connection (main menu > Target > Connection…). It is possible to use other connections, the UART is used because the mcuboot application is built with the debug console and prints the status that can be verified using the terminal.

  3. Verify the selected boot memory in main menu > Target > Boot Memory…. For MCX N series, IFR must be used.

  4. On the Build image view, select the “mcuboot opensource” application as “Source executable image”. The prebuilt application is available in sample_data\targets\<processor>\source_images\<board>_mcuboot_opensource.s19. You can also build your own from MCUXpresso SDK. If the application contains a configuration of the external flash (FCB), the tool detects and offers to use it. It is recommended to accept.

  5. Open main menu > Tools > MCUboot > Sign Image and configure the following:

    • The secondary application to be signed; the prebuilt application is available in sample_data\targets\<processor>\source_images\<board>_ota_mcuboot_basic.s19

    • The signing key; it is located in the same folder that the prebuilt application or in MCUXpresso SDK, in folder boards\<board>\ota_examples\mcuboot_opensource\keys\. Depending on the platform. use either sign-rsa2048-priv.pem or sign-ecdsa-p256-priv.pem. Keys protected by a password are not supported yet.

    • The imgtool arguments by default should match the SDK example. It is not needed to change them.

    • Click the Sign button to sign the application; fix problems, if any.

    • Ensure that the check boxes below are selected:

      • the first check-box: the tool creates the pre-build hook script that signs the application before each build

      • second check-box: the tool reconfigures additional images, so the signed image is written to the target address; keep “Image 1”

    • Verify the target address of the application.

    • Close the dialog by clicking the Save & Close button.

  6. On the Build tab, double-check that the Build script hooks section contains the pre-build script.

  7. Open Additional Images and check that the signed application is properly configured as “Image 1”.

  8. Build and write the bootable image into the processor.

  9. Open a terminal (in MCUXpresso IDE go to main menu > Windows > Show View > Other > Terminal), select the UART port, confirm, and reset the processor. You should receive the following text:

    hello sbl.
    Bootloader Version 2.0.0
    Primary   slot: version=1.0.0+0
    Image 0 Secondary slot: Image not found
    writing copy_done; fa_id=0 off=0xfffd0 (0xfffd0)
    Image 0 loaded from the primary slot
    Bootloader chainload address offset: 0x0
    Reset_Handler address offset: 0x400
    Jumping to the image
    
    Booting the primary slot - flash remapping is disabled
    
    *************************************
    * Basic MCUBoot application example *
    *************************************
    Built Apr 16 YYYY 12:34:56
    

To sign and write a second copy of the application, follow additional steps:

  1. Disconnect the terminal if it is still open. Reset the board to ISP mode.

  2. Open main menu > Tools > MCUboot > Sign Image…

  3. Keep the same input application image.

  4. Change the output image name, for example add suffix 1_1

  5. In imgtool arguments, change version to 1.1

  6. In the Set additional image section change:

    • Image 2

    • Target address - increase the address by the slot size (see the slot size parameter in the imgtool arguments)

  7. Save and Close.

    Note: The pre-build script will be overwritten and it will sign Image 2. The previously signed Image 1 remains on the disk untouched and it will be written to flash at the original location.

  8. Open Additional Images and check that there are two applications: “Image 1” and “Image 2”.

  9. Build and write.

  10. Connect the terminal, switch the board to boot from the selected boot memory, and reset. The terminal should receive the following text:

    hello sbl.
    Bootloader Version 2.0.0
    Primary   slot: version=1.0.0+0
    Secondary slot: version=1.1.0+0
    writing copy_done; fa_id=1 off=0xfffd0 (0x1fffd0)
    Image 0 loaded from the secondary slot
    Bootloader chainload address offset: 0x100000
    Reset_Handler address offset: 0x100400
    Jumping to the image
    
    Booting the secondary slot - flash remapping is enabled
    
    *************************************
    * Basic MCUBoot application example *
    *************************************
    
    Built Apr 16 YYYY 13:24:56
    

EdgeLock 2GO trust provisioning workflow#

EdgeLock 2GO is a fully managed cloud platform operated by NXP that provides secure provisioning services for easy deployment and maintenance of IoT devices using supported NXP products. The service allows creating and managing secure objects, such as symmetric keys, key-pairs, and certificates that are then securely provisioned into your NXP MCU or MPU.

The tool supports the following flows:

  • EdgeLock 2GO with device ID flow, where the manufacturing facility retrieves secure objects from EdgeLock 2GO cloud server during the production process specifically for each processor

  • EdgeLock 2GO per product type flow, where OEM retrieves secure objects database from EdgeLock 2GO server and production in manufacturing facility can operate without online access to EdgeLock 2GO server

EdgeLock 2GO with device ID, high-level description#

The figures below correspond to the sequence of actions indicated on Figure “EdgeLock 2GO trust provisioning workflow”.

Configuration process

  1. OEM prepares a secure configuration and verifies it locally. Then the SEC Tool provides all secure objects, and the OEM uploads them via the EdgeLock 2GO web portal.

  2. OEM sends to manufacturing facility manufacturing package generated from SEC Tool.

Manufacturing process for EdgeLock 2GO with device ID

  1. The tool fetches the processor UUID

  2. The tool requests secure objects for the given UUID. The EdgeLock 2GO server validates UUID, generates secure objects, and encrypts them with EdgeLock 2GO root of trust. Secure objects are downloaded to the manufacturing machine.

  3. Secure objects and EdgeLock 2GO provisioning firmware are loaded to the target processor. The firmware is invoked to install the secure objects into the target location. The application image is applied into the target boot memory.

_images/EdgeLock_2GO_Trust_Provisioning_workflow.svg

Fig. 80 EdgeLock 2GO trust provisioning workflow#

EdgeLock 2GO per product type, high-level description#

Configuration process

  1. OEM prepares a secure configuration and verifies it locally. Then the SEC Tool provides all secure objects, and the OEM uploads them via the EdgeLock 2GO web portal. Note: secure objects for device ID flow and per product flow are the same; however, at the EdgeLock 2GO web portal the device group must be created with different parameters.

  2. OEM downloads the database of secure objects and provides the database and manufacturing package to the manufacturing facility.

Manufacturing process for EdgeLock 2GO per product type

  1. The tool fetches the processor UUID and verifies in the database that it is not provisioned yet.

  2. The tool fetches secure objects from the database and records into DB UUID of the provisioned device.

  3. Secure objects and EdgeLock 2GO provisioning firmware are loaded to the target processor. The firmware is invoked to install the secure objects into the target location. The application image is applied into the target boot memory.

EdgeLock 2GO flow, step by step#

This chapter contains a detailed, step-by-step, description of the provisioning flow. The chapter is split into two phases:

  • development: description of how to test the provisioning process with irreversible changes in the processor

  • production: information on how to switch to the deployment life cycle and prepare a package for the manufacturing facility

For processor-specific information, see Processor-specific workflows.

EdgeLock 2GO flow, step by step, development#

To configure EdgeLock 2GO provisioning, do the following steps:

  1. Turn on secure boot mode and verify that the application works properly.

  2. On the EdgeLock 2GO server, create the device group for the product and create an API key. For details, see EdgeLock 2GO Configuration via web portal.

  3. In the main menu > Target > Trust Provisioning Mode, select EdgeLock 2GO. Select either EdgeLock 2GO with device ID or EdgeLock 2GO per product type. Fill the EdgeLock 2GO parameters and test the connection to the server.

  4. Install the GnuPG Tool and take advantage of the prepared encryption script.

    OS-specific notes:

    • Windows: Kleopatra for Windows is recommended: Kleopatra for Windows (GPG4Win). The encryption can also be done both manually using “Kleopatra GUI”. See EdgeLock 2GO Quick Start Guide (document AN13255 on EdgeLock 2GO server) or using the way described above (GnuPG utilities are installed with gpg4win).

    • Ubuntu: use the gpg package in the Ubuntu repositories.

    • macOS: gnupg available in the brew package system is a recommended option; GnuPG for OS X should also work (see GnuPG downloads )

  5. Steps needed to enable the GPG encryption in the build script:

    • The encryption is done in the el2go/encrypt_el2go_files_*.* script generated into the workspace. Use the Update files button on the Build page to update the script.

    • Import the EdgeLock 2GO public key for encryption, see the generated script for how to do it

    • Generate RSA key pair for signing - gpg --full-generate-key. Use 2048 or 4096 key size.

    • Set environment variables

      • EL2GO_GPG_PASSWORD - password for the generated key pair

      • EL2GO_GPG_SIGN_KEY - identify which key should be used for signing using key ID available by gpg--list-secret-keys. If the EL2GO_GPG_SIGN_KEY environment variable is defined, the encryption is invoked from the build script as a part of the build action.

  6. Ensure that the development life cycle is selected in the main menu > Target > Life Cycle. For development purposes, the EdgeLock 2GO verification is supported with the open life cycle. This is not intended for production.

  7. On the build page, click Build image to build the application. Ensure that there are no errors. Ensure the connected processor and target flash memory are clear.

  8. Open the <workspace>/el2go/publish subfolder and upload all secure assets into the EdgeLock 2GO server. Follow the instructions provided in EdgeLock 2GO Configuration via web portal.

    Note: Files for the EdgeLock 2GO server are also displayed on the build page. In the generated files, they are marked by the el2go cloud icon. The description is displayed in the tooltip.

  9. For EdgeLock 2GO per product flow, follow Create database with secure objects for EdgeLock 2GO per product type.

  10. Go to the Write page and run the Write operation.

EdgeLock 2GO flow, step by step, production#

  1. If everything works as expected, set the deployment life cycle and repeat steps 7, 8, 9, 10. Make sure that the policy for uploaded secure objects is aligned with the life cycle.

  2. If everything works as expected, create the manufacturing package. For details, see Create manufacturing package. For API key distribution, see API key to access EdgeLock 2GO server.

API key to access EdgeLock 2GO server#

  • For development, the API key must be specified in the Trust Provisioning Mode dialog.

  • For EdgeLock 2GO per product type, the API key is not used in the manufacturing

  • For EdgeLock 2GO with device ID, the API key is also needed for manufacturing:

    • For the manufacturing package, the API key can be specified optionally; if it is specified, it is recommended to encrypt the package with a password to protect the access.

    • If the API key is not specified in the manufacturing package, it can be specified in the manufacturing dialog or via the environment variable SEC_EL2GO_API_KEY.

    • For EdgeLock 2GO trust provisioning, the following access needs to be enabled for the manufacturing API key on the EdgeLock 2GO server:

      • View - View device groups

      • General - Register devices

      • Remote trust provisioning - View secure objects and their intermediate CAs

    • For EdgeLock 2GO WPC provisioning, the following access needs to be enabled for the manufacturing API key on the EdgeLock 2GO server:

      • View - View Qi related data

      • Manage - Assign and unassign Qi templates to Device Groups and query jobs for batch processing

EdgeLock 2GO configuration via web portal#

EdgeLock 2GO web portal URL: EdgeLock 2GO web portal

The following Application Note provides detailed information: EdgeLock 2GO Provisioning via Secure Provisioning Tool (SEC) for MCUs (document AN14624).

How to create a device group

  • Devices > New Device Group

  • Assign any name

  • Hardware family type: MPU and MCU

  • Hardware option: product name

  • Hardware type and product name: select a processor by name

How to create RKTH secure object

  • Secure Objects > New Secure Object

  • Select type: OEM FW Authentication Key Hash

  • Assign any name

  • Provide a binary file: <upload the file>

  • Usage policies: add a custom policy. Select the Open or Closed/Locked policy. Open is used for development and testing, Closed and Closed/Locked are used for production. The policy is to be aligned with the life cycle selected in the tool. For details, see processor-specific recommendations.

How to create CUST-MK-SK secure object

  • Secure Objects > New Secure Object

  • Select type: OEM FW Decryption Key

  • Assign any name

  • Provide the key material (.asc): provide a signed and encrypted key. It is generated by a SEC Tool via GnuPG.

  • Provide the public key to use it for verifying the signature of the encrypted key. (.asc): your public key

  • Usage policies: same as RKTH; the policy must be the same for all secure objects used in one device group.

Other secure object

See processor-specific information in Processor-specific workflows.

Database with secure objects for EdgeLock 2GO per product type#

There are two types of the databases:

  • static database: does not contain any processor specific secure objects

  • dynamic database: contains processor-specific certificates

To create a database of secure objects for “offline” provisioning (EdgeLock 2GO per product type), follow these steps:

  1. Open main menu > Targets > Trust Provisioning Mode… and ensure EdgeLock 2GO per product type is selected.

  2. In Per Product Database panel, specify:

    • number of devices per database

    • number of databases to be generated

    These parameters will be used for dynamic database only. For a static database, the parameters will be ignored.

  3. Click the button to start generation. The generation of dynamic databases may require several hours when processing a large number of processors or secure objects. A progress bar with an estimated completion time is displayed. Do not close the window until the database generation is complete.

  4. Click the Download button to download the databases from the server.

For the write operation (in development), the database name is hard-coded to <workspace>/trust_provisioning/el2go_product_batch.db. For manufacturing operation, the database name and location can be selected in the manufacturing dialog.

Databases are not included in the manufacturing package and are expected to be delivered separately.

Merge Images Tool workflow#

This section describes merging two separate images into one single image. The reason for merging might be signing both images together during the build process. This section is written for MCUXpresso IDE with the Trust zone hello world SDK example, which contains two separate projects _hello_world_s and _hello_worlds_ns linked together. It is necessary to remove the link between the projects (MCUXpresso IDE) to generate two separated images instead of one image created during the build process by merging both projects together. As an example processor the MIMXRT595 is used. For other processors the workflow is the same, except of the start addresses.

Building the TrustZone example projects for merge#

  1. Remove linking between both projects by selecting the non-secured project _hello_world_ns go to Project > Properties > Project References and unchecking the _hello_world_s from the references.

  2. Build both projects without any modifications

  3. This example uses .s19 files so the final .axf files need to be converted. To do so, go to the Debug folder for both projects, right-click the generated _hello_world_*.axf file, and choose Binary Utilities > Create S-Record.

Merging two images into one#

  1. Open the Merge Tool by selecting main menu > Tools > Merge Tool.

  2. Select _hello_world_s.s19. The target address will be automatically set to 0x18001000 (secured memory area)

  3. For MIMXRT595 processors, only the non-secured address can be written by the user. The given address of the first image is in the secured memory map. Change the target address of the first image to 0x08001000 (non-secured memory area)

  4. Select _hello_world_ns.s19. The target address will be automatically set to 0x08100000 (non-secured memory area)

  5. Check the Apply the merged images as the Source executable image on Build image view checkbox

  6. Leave the rest as it is and press the OK button

  7. Check that the image is automatically applied as a Source executable image and its start address is updated as well

Signing merged image#

To sign and build the merged image, see the Booting signed image using shadow registers section, but use the merged image as a Source executable image instead.

Custom USB VID and PID devices workflow#

If you have a device with custom VID&PID, it is possible to select the custom VID&PID in the main menu > Target > Connection. Selected VID&PID is used for the whole write operation. Write script does not support a change of VID&PID during its execution. It is recommended to change VID&PID prior to the write operation (for example, using PFR configuration or OTP configuration in Advanced mode), reset the processor and then start the write operation with custom VID&PID.

For manufacturing operation, custom VID&PID must be selected in the Connection configuration during the creation of the manufacturing package. With such configuration, the manufacturing operation accepts both default and custom VID&PID.