![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The frdm_kl25z.c file defines GPIO pins for FRDM-KL25Z board. More...
#include "frdm_kl25z.h"
Go to the source code of this file.
Functions | |
| uint32_t | UART0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | UART2_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | SPI0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | SPI1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The frdm_kl25z.c file defines GPIO pins for FRDM-KL25Z board.
Definition in file frdm_kl25z.c.
| uint32_t I2C0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 297 of file frdm_kl25z.c.
| uint32_t I2C1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 309 of file frdm_kl25z.c.
| uint32_t SPI0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 321 of file frdm_kl25z.c.
| uint32_t SPI1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 333 of file frdm_kl25z.c.
| uint32_t UART0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 260 of file frdm_kl25z.c.
| uint32_t UART1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 273 of file frdm_kl25z.c.
| uint32_t UART2_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 285 of file frdm_kl25z.c.
Definition at line 114 of file frdm_kl25z.c.
Definition at line 121 of file frdm_kl25z.c.
Definition at line 128 of file frdm_kl25z.c.
Definition at line 66 of file frdm_kl25z.c.
Definition at line 59 of file frdm_kl25z.c.
| gpioHandleKSDK_t ACCEL_SCL |
Definition at line 223 of file frdm_kl25z.c.
| gpioHandleKSDK_t ACCEL_SDA |
Definition at line 230 of file frdm_kl25z.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 214 of file frdm_kl25z.c.
Definition at line 98 of file frdm_kl25z.c.
Definition at line 105 of file frdm_kl25z.c.
| gpioHandleKSDK_t D10 |
Definition at line 191 of file frdm_kl25z.c.
| gpioHandleKSDK_t D11 |
Definition at line 82 of file frdm_kl25z.c.
| gpioHandleKSDK_t D12 |
Definition at line 89 of file frdm_kl25z.c.
| gpioHandleKSDK_t D13 |
Definition at line 75 of file frdm_kl25z.c.
| gpioHandleKSDK_t D14 |
Definition at line 50 of file frdm_kl25z.c.
| gpioHandleKSDK_t D15 |
Definition at line 43 of file frdm_kl25z.c.
Definition at line 135 of file frdm_kl25z.c.
Definition at line 142 of file frdm_kl25z.c.
Definition at line 149 of file frdm_kl25z.c.
Definition at line 156 of file frdm_kl25z.c.
Definition at line 163 of file frdm_kl25z.c.
Definition at line 170 of file frdm_kl25z.c.
Definition at line 177 of file frdm_kl25z.c.
Definition at line 184 of file frdm_kl25z.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 207 of file frdm_kl25z.c.
| gpioHandleKSDK_t INT1 |
Definition at line 238 of file frdm_kl25z.c.
| gpioHandleKSDK_t INT2 |
Definition at line 245 of file frdm_kl25z.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 200 of file frdm_kl25z.c.