![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
#include "Driver_Common.h"#include "Driver_GPIO.h"#include "fsl_common.h"#include "fsl_gpio.h"#include "fsl_port.h"

Go to the source code of this file.
Data Structures | |
| struct | gpioConfigKSDK |
| The GPIO Configuration KSDK. More... | |
| struct | gpioHandleKSDK |
| The GPIO pin handle for KSDK. More... | |
| struct | gpioIsrObj |
| The gpio isr object. More... | |
Macros | |
| #define | MAKE_GPIO_HANDLE(PortName, Base, PortBase, PinNumber, Irq, ClockName, PortNumber) |
| Macro to create a Gpio handle. More... | |
| #define | GPIO_PIN_ID(PortName, PinNumber) &(PortName##PinNumber) |
Typedefs | |
| typedef enum port_number | port_number_t |
| GPIO PORT NAMES. More... | |
| typedef struct gpioConfigKSDK | gpioConfigKSDK_t |
| The GPIO Configuration KSDK. More... | |
| typedef struct gpioHandleKSDK | gpioHandleKSDK_t |
| The GPIO pin handle for KSDK. More... | |
| typedef struct gpioIsrObj | gpioIsrObj_t |
| The gpio isr object. More... | |
Enumerations | |
| enum | port_number { GPIO1_NUM = 0, GPIO2_NUM = 1, GPIO3_NUM = 2, GPIO4_NUM = 3, GPIO5_NUM = 4, TOTAL_NUMBER_PORT, PORTA_NUM = 0, PORTB_NUM = 1, PORTC_NUM = 2, PORTD_NUM = 3, PORTE_NUM = 4, TOTAL_NUMBER_PORT, PORTA_NUM = 0, PORTB_NUM = 1, TOTAL_NUMBER_PORT } |
| GPIO PORT NAMES. More... | |
Variables | |
| GENERIC_DRIVER_GPIO | Driver_GPIO_KSDK |
| #define GPIO_PIN_ID | ( | PortName, | |
| PinNumber | |||
| ) | &(PortName##PinNumber) |
Definition at line 107 of file gpio_driver.h.
| #define MAKE_GPIO_HANDLE | ( | PortName, | |
| Base, | |||
| PortBase, | |||
| PinNumber, | |||
| Irq, | |||
| ClockName, | |||
| PortNumber | |||
| ) |
Macro to create a Gpio handle.
Definition at line 98 of file gpio_driver.h.
| typedef struct gpioConfigKSDK gpioConfigKSDK_t |
The GPIO Configuration KSDK.
| typedef struct gpioHandleKSDK gpioHandleKSDK_t |
The GPIO pin handle for KSDK.
| typedef struct gpioIsrObj gpioIsrObj_t |
The gpio isr object.
| typedef enum port_number port_number_t |
GPIO PORT NAMES.
| enum port_number |
GPIO PORT NAMES.
| Enumerator | |
|---|---|
| GPIO1_NUM | |
| GPIO2_NUM | |
| GPIO3_NUM | |
| GPIO4_NUM | |
| GPIO5_NUM | |
| TOTAL_NUMBER_PORT | |
| PORTA_NUM | |
| PORTB_NUM | |
| PORTC_NUM | |
| PORTD_NUM | |
| PORTE_NUM | |
| TOTAL_NUMBER_PORT | |
| PORTA_NUM | |
| PORTB_NUM | |
| TOTAL_NUMBER_PORT | |
Definition at line 52 of file gpio_driver.h.
| GENERIC_DRIVER_GPIO Driver_GPIO_KSDK |
Definition at line 203 of file gpio_driver.c.