ISSDK  1.7
IoT Sensing Software Development Kit
Data Structures | Macros | Functions
mma9553_drv.h File Reference

The mma9553_drv.h file describes the MMA9553L driver interface and structures. More...

#include <stdint.h>
#include "mma9553.h"
#include "sensor_io_i2c.h"
#include "sensor_io_spi.h"
#include "register_io_i2c.h"
#include "register_io_spi.h"
Include dependency graph for mma9553_drv.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  mma9553_spi_sensorhandle_t
 This defines the sensor specific information for SPI. More...
 
struct  mma9553_i2c_sensorhandle_t
 This defines the sensor specific information for I2C. More...
 
struct  mma9553_acceldata_t
 This structure defines the mma9553 pedometer data buffer. More...
 
struct  mma9553_pedometerdata_t
 This structure defines the Size of response for pedometer data read command. More...
 

Macros

#define MMA9553_COCO_ERROR_MASK   (0x7F)
 The Error Bit Mask in COCO Byte. More...
 
#define MMA9553_SPI_MAX_MSG_SIZE   (64)
 The MAX size of SPI message. More...
 
#define MMA9553_SPI_CMD_LEN   (1)
 The size of the Sensor specific SPI Header. More...
 
#define MMA9553_SS_ACTIVE_VALUE   SPI_SS_ACTIVE_LOW
 Is the Slave Select Pin Active Low or High. More...
 

Functions

int32_t MMA9553_I2C_Initialize (mma9553_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress)
 The interface function to initialize the sensor. More...
 
void MMA9553_I2C_SetIdleTask (mma9553_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the I2C Idle Task. More...
 
int32_t MMA9553_I2C_Configure (mma9553_i2c_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList)
 The interface function to configure he sensor. More...
 
int32_t MMA9553_I2C_CommandResponse (mma9553_i2c_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t MMA9553_I2C_DeInit (mma9553_i2c_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 
int32_t MMA9553_SPI_Initialize (mma9553_spi_sensorhandle_t *pSensorHandle, ARM_DRIVER_SPI *pBus, uint8_t index, void *pSlaveSelect, void *pReset)
 The interface function to initialize the sensor. More...
 
void MMA9553_SPI_SetIdleTask (mma9553_spi_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
 : The interface function to set the SPI Idle Task. More...
 
int32_t MMA9553_SPI_Configure (mma9553_spi_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList)
 The interface function to configure he sensor. More...
 
int32_t MMA9553_SPI_CommandResponse (mma9553_spi_sensorhandle_t *pSensorHandle, const registercommandlist_t *pCommandList, const registerreadlist_t *pReadList, uint8_t *pBuffer)
 The interface function to read the sensor data. More...
 
int32_t MMA9553_SPI_DeInit (mma9553_spi_sensorhandle_t *pSensorHandle)
 The interface function to De Initialize sensor.. More...
 
void MMA9553_SPI_ReadPreprocess (void *pCmdOut, uint32_t offset, uint32_t size)
 The SPI Read Pre-Process function to generate Sensor specific SPI Message Header. More...
 
void MMA9553_SPI_WritePreprocess (void *pCmdOut, uint32_t offset, uint32_t size, void *pWritebuffer)
 The SPI Write Pre-Process function to generate Sensor specific SPI Message Header. More...
 

Detailed Description

The mma9553_drv.h file describes the MMA9553L driver interface and structures.

Definition in file mma9553_drv.h.

Macro Definition Documentation

◆ MMA9553_COCO_ERROR_MASK

#define MMA9553_COCO_ERROR_MASK   (0x7F)

◆ MMA9553_SPI_CMD_LEN

#define MMA9553_SPI_CMD_LEN   (1)

The size of the Sensor specific SPI Header.

Definition at line 107 of file mma9553_drv.h.

Referenced by MMA9553_SPI_Initialize(), MMA9553_SPI_ReadPreprocess(), and MMA9553_SPI_WritePreprocess().

◆ MMA9553_SPI_MAX_MSG_SIZE

#define MMA9553_SPI_MAX_MSG_SIZE   (64)

The MAX size of SPI message.

Definition at line 103 of file mma9553_drv.h.

◆ MMA9553_SS_ACTIVE_VALUE

#define MMA9553_SS_ACTIVE_VALUE   SPI_SS_ACTIVE_LOW

Is the Slave Select Pin Active Low or High.

Definition at line 111 of file mma9553_drv.h.

Referenced by MMA9553_SPI_Initialize().

Function Documentation

◆ MMA9553_I2C_CommandResponse()

int32_t MMA9553_I2C_CommandResponse ( mma9553_i2c_sensorhandle_t *  pSensorHandle,
const registercommandlist_t *  pCommandList,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pCommandListpointer to the command read list.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after MMA9553_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
MMA9553_I2C_CommandResponse() returns the status .

Validate for the correct handle and register read list.

Check whether sensor handle is initialized before reading sensor data.

Definition at line 513 of file mma9553_drv.c.

References mma9553_i2c_sensorhandle_t::deviceInfo, int32_t(), mma9553_i2c_sensorhandle_t::isInitialized, MMA9553_COCO_ERROR_MASK, mma9553_i2c_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, SENSOR_ERROR_WRITE, Sensor_I2C_BlockWrite(), Sensor_I2C_Read(), mma9553_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ MMA9553_I2C_Configure()

int32_t MMA9553_I2C_Configure ( mma9553_i2c_sensorhandle_t *  pSensorHandle,
const registercommandlist_t *  pCommandList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pCommandListpointer to the command write list.
Constraints:
This can be called any number of times only after MMA9553_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
MMA9553_I2C_Configure() returns the status.

Check whether sensor handle is initialized before applying configuration.

Definition at line 448 of file mma9553_drv.c.

References mma9553_i2c_sensorhandle_t::deviceInfo, int32_t(), mma9553_i2c_sensorhandle_t::isInitialized, MMA9553_COCO_ERROR_MASK, MMA9553_HDR_SIZE, mma9553_i2c_sensorhandle_t::pCommDrv, Register_I2C_Read(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_READ, SENSOR_ERROR_WRITE, Sensor_I2C_BlockWrite(), mma9553_i2c_sensorhandle_t::slaveAddress, STANDBY_REG_SIZE, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ MMA9553_I2C_DeInit()

int32_t MMA9553_I2C_DeInit ( mma9553_i2c_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after MMA9553_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
MMA9553_I2C_DeInit() returns the status .

Check whether sensor handle is initialized before triggering sensor reset.

De-initialize sensor handle.

Definition at line 555 of file mma9553_drv.c.

References mma9553_i2c_sensorhandle_t::deviceInfo, int32_t(), mma9553_i2c_sensorhandle_t::isInitialized, MMA9553_COCO_ERROR_MASK, mma9553_i2c_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_I2C_BlockWrite(), mma9553_i2c_sensorhandle_t::slaveAddress, and status.

Here is the call graph for this function:

◆ MMA9553_I2C_Initialize()

int32_t MMA9553_I2C_Initialize ( mma9553_i2c_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_I2C *  pBus,
uint8_t  index,
uint16_t  sAddress 
)

The interface function to initialize the sensor.

This function initialize the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible I2C bus object.
[in]indexthe I2C device number.
[in]sAddressslave address of the device on the bus.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
MMA9553_I2C_Initialize() returns the status .

Check the input parameters.

Definition at line 395 of file mma9553_drv.c.

References BOARD_DELAY_ms(), mma9553_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, registerDeviceInfo_t::functionParam, registerDeviceInfo_t::idleFunction, int32_t(), mma9553_i2c_sensorhandle_t::isInitialized, MMA9553_COCO_ERROR_MASK, MMA9553_HDR_SIZE, mma9553_i2c_sensorhandle_t::pCommDrv, ReadVersionInfo, Register_I2C_BlockWrite(), Register_I2C_Read(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_I2C_BlockWrite(), mma9553_i2c_sensorhandle_t::slaveAddress, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ MMA9553_I2C_SetIdleTask()

void MMA9553_I2C_SetIdleTask ( mma9553_i2c_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the I2C Idle Task.

Parameters
[in]mma9553_i2c_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on I2C Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after MMA9553_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 440 of file mma9553_drv.c.

References mma9553_i2c_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ MMA9553_SPI_CommandResponse()

int32_t MMA9553_SPI_CommandResponse ( mma9553_spi_sensorhandle_t *  pSensorHandle,
const registercommandlist_t *  pCommandList,
const registerreadlist_t *  pReadList,
uint8_t *  pBuffer 
)

The interface function to read the sensor data.

This function read the sensor data out from the device and returns raw data in a byte stream.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pCommandListpointer to the command read list.
[in]pReadListpointer to the list of device registers and values to read.
[out]pBufferbuffer which holds raw sensor data.This buffer may be back to back databuffer based command read in the list.
Constraints:
This can be called any number of times only after MMA9553_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
MMA9553_SPI_CommandResponse() returns the status .

Validate for the correct handle and command list.

Check whether sensor handle is initialized before reading sensor data.

Parse through the read list and read the data one by one.

Definition at line 321 of file mma9553_drv.c.

References mma9553_spi_sensorhandle_t::deviceInfo, int32_t(), mma9553_spi_sensorhandle_t::isInitialized, MMA9553_COCO_ERROR_MASK, mma9553_spi_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_READ, SENSOR_ERROR_WRITE, Sensor_SPI_BlockWrite(), Sensor_SPI_Read(), mma9553_spi_sensorhandle_t::slaveParams, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ MMA9553_SPI_Configure()

int32_t MMA9553_SPI_Configure ( mma9553_spi_sensorhandle_t *  pSensorHandle,
const registercommandlist_t *  pCommandList 
)

The interface function to configure he sensor.

This function configure the sensor with requested ODR, Range and registers in the regsiter pair array.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pCommandListpointer to the command list.
Constraints:
This can be called any number of times only after FXAS21002_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
MMA9553_SPI_Configure() returns the status .

Validate for the correct handle and register write list.

Check whether sensor handle is initialized before applying configuration.

Definition at line 256 of file mma9553_drv.c.

References mma9553_spi_sensorhandle_t::deviceInfo, int32_t(), mma9553_spi_sensorhandle_t::isInitialized, MMA9553_COCO_ERROR_MASK, MMA9553_HDR_SIZE, mma9553_spi_sensorhandle_t::pCommDrv, Register_SPI_Read(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_READ, SENSOR_ERROR_WRITE, Sensor_SPI_BlockWrite(), mma9553_spi_sensorhandle_t::slaveParams, STANDBY_REG_SIZE, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ MMA9553_SPI_DeInit()

int32_t MMA9553_SPI_DeInit ( mma9553_spi_sensorhandle_t *  pSensorHandle)

The interface function to De Initialize sensor..

This function made sensor in a power safe state and de initialize its handle.

Parameters
[in]pSensorHandlehandle to the sensor.
Constraints:
This can be called only after after MMA9553_SPI_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
MMA9553_SPI_DeInit() returns the status .

Check whether sensor handle is initialized before triggering sensor reset.

Trigger sensor device reset.

De-initialize sensor handle.

Definition at line 364 of file mma9553_drv.c.

References mma9553_spi_sensorhandle_t::deviceInfo, int32_t(), mma9553_spi_sensorhandle_t::isInitialized, MMA9553_COCO_ERROR_MASK, mma9553_spi_sensorhandle_t::pCommDrv, SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_SPI_BlockWrite(), mma9553_spi_sensorhandle_t::slaveParams, and status.

Here is the call graph for this function:

◆ MMA9553_SPI_Initialize()

int32_t MMA9553_SPI_Initialize ( mma9553_spi_sensorhandle_t *  pSensorHandle,
ARM_DRIVER_SPI *  pBus,
uint8_t  index,
void *  pSlaveSelect,
void *  pReset 
)

The interface function to initialize the sensor.

This function initializes the sensor and sensor handle.

Parameters
[in]pSensorHandlehandle to the sensor.
[in]pBuspointer to the CMSIS API compatible SPI bus object.
[in]indexthe I2C device number.
[in]pSlaveSelectslave select hndle of the device on the bus.
[in]pResetreset handle of the device on the bus.
Constraints:
This should be the first API to be called. Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
MMA9553_SPI_Initialize() returns the status .

Check the input parameters.

Initialize the sensor handle.

Definition at line 183 of file mma9553_drv.c.

References BOARD_DELAY_ms(), GENERIC_DRIVER_GPIO::clr_pin, mma9553_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::deviceInstance, Driver_GPIO_KSDK, registerDeviceInfo_t::functionParam, GPIO_DIRECTION_OUT, registerDeviceInfo_t::idleFunction, int32_t(), mma9553_spi_sensorhandle_t::isInitialized, MMA9553_COCO_ERROR_MASK, MMA9553_HDR_SIZE, MMA9553_SPI_CMD_LEN, MMA9553_SPI_ReadPreprocess(), MMA9553_SPI_WritePreprocess(), MMA9553_SS_ACTIVE_VALUE, mma9553_spi_sensorhandle_t::pCommDrv, pGPIODriver, GENERIC_DRIVER_GPIO::pin_init, spiSlaveSpecificParams_t::pReadPreprocessFN, spiSlaveSpecificParams_t::pTargetSlavePinID, spiSlaveSpecificParams_t::pWritePreprocessFN, ReadVersionInfo, Register_SPI_BlockWrite(), Register_SPI_Read(), SENSOR_ERROR_INIT, SENSOR_ERROR_INVALID_PARAM, SENSOR_ERROR_NONE, SENSOR_ERROR_WRITE, Sensor_SPI_BlockWrite(), GENERIC_DRIVER_GPIO::set_pin, mma9553_spi_sensorhandle_t::slaveParams, spiSlaveSpecificParams_t::spiCmdLen, spiSlaveSpecificParams_t::ssActiveValue, and status.

Referenced by main().

Here is the call graph for this function:
Here is the caller graph for this function:

◆ MMA9553_SPI_ReadPreprocess()

void MMA9553_SPI_ReadPreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size 
)

The SPI Read Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Read Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start reading from.
[in]sizenumber of bytes to read.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 146 of file mma9553_drv.c.

References MMA9553_SPI_CMD_LEN, mma9553_spiRead_CmdBuffer, mma9553_spiRead_DataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by MMA9553_SPI_Initialize().

Here is the caller graph for this function:

◆ MMA9553_SPI_SetIdleTask()

void MMA9553_SPI_SetIdleTask ( mma9553_spi_sensorhandle_t *  pSensorHandle,
registeridlefunction_t  idleTask,
void *  userParam 
)

: The interface function to set the SPI Idle Task.

Parameters
[in]mma9553_spi_sensorhandle_t *pSensorHandle, handle to the sensor handle.
[in]registeridlefunction_t idleTask, function pointer to the function to execute on SPI Idle Time.
[in]void *userParam, the pointer to the user idle ftask parameters.
Returns
void.
Constraints:
This can be called any number of times only after MMA9553_I2C_Initialize(). Application has to ensure that previous instances of these APIs have exited before invocation. No

Definition at line 248 of file mma9553_drv.c.

References mma9553_spi_sensorhandle_t::deviceInfo, registerDeviceInfo_t::functionParam, and registerDeviceInfo_t::idleFunction.

Referenced by main().

Here is the caller graph for this function:

◆ MMA9553_SPI_WritePreprocess()

void MMA9553_SPI_WritePreprocess ( void *  pCmdOut,
uint32_t  offset,
uint32_t  size,
void *  pWritebuffer 
)

The SPI Write Pre-Process function to generate Sensor specific SPI Message Header.

This function prepares the SPI Write Command Header with register address and R/W bit encoded as the Sensor.

Parameters
[out]pCmdOuthandle to the output buffer.
[in]offsetthe address of the register to start writing from.
[in]sizenumber of bytes to write.
Constraints:
None Application has to ensure that previous instances of these APIs have exited before invocation. No
Returns
:: None.

Definition at line 163 of file mma9553_drv.c.

References MMA9553_SPI_CMD_LEN, mma9553_spiWrite_CmdDataBuffer, spi_mater_SlaveCmd::pReadBuffer, spi_mater_SlaveCmd::pWriteBuffer, and spi_mater_SlaveCmd::size.

Referenced by MMA9553_SPI_Initialize().

Here is the caller graph for this function: