35 #ifndef SENSOR_FUSION_STATUS_H_ 36 #define SENSOR_FUSION_STATUS_H_ void() ssUpdateStatus_t(struct StatusSubsystem *pStatus)
fusion_status_t previous
Previous status state - fusion_status_t is defined in sensor_fusion.h.
void initializeStatusSubsystem(StatusSubsystem *pStatus)
struct StatusSubsystem StatusSubsystem
StatusSubsystem() provides an object-like interface for communicating status to the user...
StatusSubsystem() provides an object-like interface for communicating status to the user...
ssUpdateStatus_t * update
make pending status active/visible
uint8_t toggle
This implementation can change LED color and have either solid/toggle.
fusion_status_t status
Current status.
ssSetStatus_t * queue
queue status change for next regular interval
ssUpdateStatus_t * test
unit test which simply increments to next state
fusion_status_t
Application-specific serial communications system.
void() ssSetStatus_t(struct StatusSubsystem *pStatus, fusion_status_t status)
fusion_status_t next
Pending status change.