ISSDK  1.7
IoT Sensing Software Development Kit
Data Fields
_comm_interface_ Struct Reference

#include <comm_interface.h>

Collaboration diagram for _comm_interface_:
Collaboration graph

Data Fields

COMM_GetCapabilities_t * GetCapabilities
 
COMM_Init_t * Init
 
COMM_Config_t * Configure
 
COMM_Send_t * Send
 
COMM_Receive_t * Receive
 
COMM_GetStatus_t * GetStatus
 

Detailed Description

Definition at line 104 of file comm_interface.h.

Field Documentation

◆ Configure

COMM_Config_t* Configure

Pointer to the communication Configure() function.

Definition at line 108 of file comm_interface.h.

Referenced by HOST_Configure().

◆ GetCapabilities

COMM_GetCapabilities_t* GetCapabilities

Pointer to the communication GetCapabilities() function.

Definition at line 106 of file comm_interface.h.

◆ GetStatus

COMM_GetStatus_t* GetStatus

Pointer to the adapter GetStatus() function.

Definition at line 111 of file comm_interface.h.

◆ Init

COMM_Init_t* Init

Pointer to the communication Initialize() function.

Definition at line 107 of file comm_interface.h.

Referenced by HOST_Initialize().

◆ Receive

COMM_Receive_t* Receive

Pointer to the communication receive() function.

Definition at line 110 of file comm_interface.h.

Referenced by HOST_Receive(), and JSON_BlockDataRead_BlockingCall().

◆ Send

COMM_Send_t* Send

Pointer to the communication send() function.

Definition at line 109 of file comm_interface.h.

Referenced by HOST_Send().


The documentation for this struct was generated from the following file: