![]() |
ISSDK
1.7
IoT Sensing Software Development Kit
|
The comm_interface.h file describes the interface definition for the communication interface. Each commaunication instance needs to implement comm interface. More...
#include <stddef.h>#include <stdint.h>#include <stdbool.h>

Go to the source code of this file.
Data Structures | |
| struct | _comm_handle_ |
| struct | _comm_control_ |
| struct | _comm_interface_ |
Macros | |
| #define | COMM_INTERFACE_OK 0 |
| Operation succeeded. More... | |
Typedefs | |
| typedef struct _comm_handle_ | comm_handle_t |
| typedef struct _comm_control_ | comm_control_t |
| typedef enum _comm_type_ | comm_type_t |
| typedef enum _comm_instance_type_ | comm_instance_type_t |
| typedef void(* | COMM_Event_t) (uint32_t event) |
| typedef int32_t() | COMM_GetCapabilities_t(comm_handle_t *pHandle) |
| The interface function to get the capability of the communication interface. More... | |
| typedef int32_t() | COMM_Init_t(comm_handle_t *pHandle, void *pCommInstance, COMM_Event_t event, void *pInitializeData) |
| The interface function to initialize the communication interface. More... | |
| typedef int32_t() | COMM_Config_t(comm_handle_t *pHandle, void *pConfigData) |
| The interface function to configure the communication interface. More... | |
| typedef int32_t() | COMM_Send_t(comm_handle_t *pHandle, void *pData, uint32_t size) |
| The interface function to send data through the communication interface. More... | |
| typedef int32_t() | COMM_Receive_t(comm_handle_t *pHandle, void *pData, uint32_t size) |
| The interface function to receive data through the communication interface. More... | |
| typedef int32_t() | COMM_GetStatus_t(comm_handle_t *pHandle) |
| The interface function to get the status of the comm. More... | |
| typedef struct _comm_interface_ | comm_interface_t |
Enumerations | |
| enum | _comm_type_ { COMM_UART, COMM_BLUETOOTH, COMM_I2C, COMM_SOCKET, COMM_NFC } |
| enum | _comm_instance_type_ { COMM_BLOCKING, COMM_NONBLOCKING } |
The comm_interface.h file describes the interface definition for the communication interface. Each commaunication instance needs to implement comm interface.
Definition in file comm_interface.h.
| #define COMM_INTERFACE_OK 0 |
Operation succeeded.
Definition at line 46 of file comm_interface.h.
Referenced by COMM_UART_GetCapabilities(), and COMM_UART_Init().
| typedef int32_t() COMM_Config_t(comm_handle_t *pHandle, void *pConfigData) |
The interface function to configure the communication interface.
Definition at line 94 of file comm_interface.h.
| typedef struct _comm_control_ comm_control_t |
| typedef void(* COMM_Event_t) (uint32_t event) |
Definition at line 88 of file comm_interface.h.
| typedef int32_t() COMM_GetCapabilities_t(comm_handle_t *pHandle) |
The interface function to get the capability of the communication interface.
Definition at line 90 of file comm_interface.h.
| typedef int32_t() COMM_GetStatus_t(comm_handle_t *pHandle) |
The interface function to get the status of the comm.
Definition at line 100 of file comm_interface.h.
| typedef struct _comm_handle_ comm_handle_t |
| typedef int32_t() COMM_Init_t(comm_handle_t *pHandle, void *pCommInstance, COMM_Event_t event, void *pInitializeData) |
The interface function to initialize the communication interface.
Definition at line 92 of file comm_interface.h.
| typedef enum _comm_instance_type_ comm_instance_type_t |
| typedef struct _comm_interface_ comm_interface_t |
| typedef int32_t() COMM_Receive_t(comm_handle_t *pHandle, void *pData, uint32_t size) |
The interface function to receive data through the communication interface.
Definition at line 98 of file comm_interface.h.
| typedef int32_t() COMM_Send_t(comm_handle_t *pHandle, void *pData, uint32_t size) |
The interface function to send data through the communication interface.
Definition at line 96 of file comm_interface.h.
| typedef enum _comm_type_ comm_type_t |
| enum _comm_instance_type_ |
| Enumerator | |
|---|---|
| COMM_BLOCKING | |
| COMM_NONBLOCKING | |
Definition at line 81 of file comm_interface.h.
| enum _comm_type_ |
| Enumerator | |
|---|---|
| COMM_UART | |
| COMM_BLUETOOTH | |
| COMM_I2C | |
| COMM_SOCKET | |
| COMM_NFC | |
Definition at line 70 of file comm_interface.h.