|  | ISSDK
    1.7
    IoT Sensing Software Development Kit | 
This structure defines the mag3110 data buffer. More...

| Data Fields | |
| uint32_t | timestamp | 
| int16_t | mag [3] | 
| int16_t | temp | 
This structure defines the mag3110 data buffer.
Definition at line 76 of file mag3110_demo.c.
| int16_t mag | 
Sensor Magnetic Strength output: signed 16-bits.
Definition at line 79 of file mag3110_demo.c.
Referenced by main().
| int16_t temp | 
| uint32_t timestamp | 
Time stamp value in micro-seconds.
Definition at line 78 of file mag3110_demo.c.
Referenced by main().