46 #include "clock_config.h"    51 #include "Driver_I2C.h"    52 #include "Driver_USART.h"    57 #include "issdk_hal.h"    58 #include "gpio_driver.h"    62 #include "auto_detection_service.h"    67 #define MAG3110_DATA_SIZE 6             68 #define MAG3110_STREAM_DATA_SIZE 12     71 #define APPLICATION_NAME "MAG3110 Magnetometer Demo"    73 #define APPLICATION_VERSION "2.5"   121     uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, 
size_t *hostMsgSize, 
size_t respBufferSize)
   123     bool success = 
false;
   138         if (respBufferSize >= boardNameLen + shieldNameLen + appNameLen + 3)
   147         hostResponse[*hostMsgSize] = appNameLen;
   150         memcpy(hostResponse + *hostMsgSize, 
embAppName, appNameLen);
   151         *hostMsgSize += appNameLen;
   153         hostResponse[*hostMsgSize] = boardNameLen;
   156         memcpy(hostResponse + *hostMsgSize, 
boardString, boardNameLen);
   157         *hostMsgSize += boardNameLen;
   159         hostResponse[*hostMsgSize] = shieldNameLen;
   162         memcpy(hostResponse + *hostMsgSize, 
shieldString, shieldNameLen);
   163         *hostMsgSize += shieldNameLen;
   173         switch (hostCommand[0]) 
   232     if (ARM_DRIVER_OK != status)
   238     status = pI2cDriver->PowerControl(ARM_POWER_FULL);
   239     if (ARM_DRIVER_OK != status)
   245     status = pI2cDriver->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);
   246     if (ARM_DRIVER_OK != status)
   253     if (ARM_DRIVER_OK != status)
   259     status = pUartDriver->PowerControl(ARM_POWER_FULL);
   260     if (ARM_DRIVER_OK != status)
   267     if (ARM_DRIVER_OK != status)
   326         if (ARM_DRIVER_OK != status)
   335         rawData.
mag[0] = ((int16_t)data[0] << 8) | data[1];
   336         rawData.
mag[1] = ((int16_t)data[2] << 8) | data[3];
   337         rawData.
mag[2] = ((int16_t)data[4] << 8) | data[5];
   342         rawData.
temp = tempdata;
 
uint32_t BOARD_SystickElapsedTime_us(int32_t *pStart)
Function to compute the Elapsed Time. 
volatile bool bStreamingEnabled
int32_t MAG3110_I2C_Initialize(mag3110_i2c_sensorhandle_t *pSensorHandle, ARM_DRIVER_I2C *pBus, uint8_t index, uint16_t sAddress, uint8_t whoAmi)
The interface function to initialize the sensor. 
#define __END_WRITE_DATA__
char boardString[ADS_MAX_STRING_LENGTH]
#define HOST_PRO_CMD_W_CFG_TAG
#define MAG3110_CTRL_REG1_DR_ODR_2
#define HOST_S_SIGNAL_EVENT
#define MAG3110_CTRL_REG2_MAG_RST_EN
void Host_IO_Receive(host_cmd_proc_fn_t process_host_command, uint8_t encoding)
void(* pin_init)(pinID_t aPinId, gpio_direction_t dir, void *apPinConfig, gpio_isr_handler_t aIsrHandler, void *apUserData)
#define BOARD_BootClockRUN
const registerwritelist_t cMag3110ConfigNormal[]
Register settings for Normal (non buffered) mode. 
int32_t MAG3110_I2C_Configure(mag3110_i2c_sensorhandle_t *pSensorHandle, const registerwritelist_t *pRegWriteList)
The interface function to configure he sensor. 
The mag3110_drv.h file describes the MAG3110 driver interface and structures. 
#define MAG3110_STREAM_DATA_SIZE
This defines the sensor specific information. 
uint8_t data[FXLS8962_DATA_SIZE]
int main(void)
Main function. 
char shieldString[ADS_MAX_STRING_LENGTH]
void(* toggle_pin)(pinID_t aPinId)
This structure defines the mag3110 data buffer. 
ARM_DRIVER_I2C * pCommDrv
char embAppName[ADS_MAX_STRING_LENGTH]
#define ADS_MAX_STRING_LENGTH
#define MAG3110_CTRL_REG1_OS_OSR_32
#define HOST_PRO_INT_DEV_TAG
uint8_t streamingPacket[STREAMING_HEADER_LEN+FXLS8962_STREAM_DATA_SIZE]
void(* registeridlefunction_t)(void *userParam)
This is the register idle function type. 
#define MAG3110_CTRL_REG1_OS_MASK
#define HOST_PRO_INT_CMD_TAG
Bit aligned values for Host Protocol Interface IDs (Bits 5-6). 
#define MAG3110_CTRL_REG2_RAW_RAW
#define __END_READ_DATA__
#define APPLICATION_VERSION
Version to distinguish between instances the same application based on target Shield and updates...
void MAG3110_I2C_SetIdleTask(mag3110_i2c_sensorhandle_t *pSensorHandle, registeridlefunction_t idleTask, void *userParam)
: The interface function to set the I2C Idle Task. 
gpioHandleKSDK_t GREEN_LED
#define MAG3110_DR_STATUS_ZYXDR_MASK
#define MAG3110_DATA_SIZE
void MAG3110_CalibrateHardIronOffset(int16_t *xValue, int16_t *yValue, int16_t *zValue)
Calibrates the magnetometer reading by determining the current hard iron offset. 
#define MAG3110_CTRL_REG1_DR_MASK
#define MAG3110_CTRL_REG2_MAG_RST_MASK
const registerreadlist_t cMag3110Status[]
Address of Status Register. 
#define MAG3110_CTRL_REG2_RAW_MASK
void Host_IO_Add_ISO_Header(uint8_t streamID, uint8_t *pStreamingPacket, size_t sizePayload)
void Host_IO_Send(uint8_t *pMsg, size_t size, uint8_t encoding)
#define APPLICATION_NAME
Unique Name for this application which should match the target GUI pkg name. 
void(* clr_pin)(pinID_t aPinId)
void BOARD_SystickEnable(void)
Function to enable systicks framework. 
#define MAG3110_CTRL_REG2_AUTO_MSRT_EN_EN
#define I2C_S_DEVICE_INDEX
GENERIC_DRIVER_GPIO * pGpioDriver
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK
#define BOARD_DEBUG_UART_BAUDRATE
bool process_host_command(uint8_t tag, uint8_t *hostCommand, uint8_t *hostResponse, size_t *hostMsgSize, size_t respBufferSize)
registerDeviceInfo_t deviceInfo
Access structure of the GPIO Driver. 
void BOARD_SystickStart(int32_t *pStart)
Function to Record the Start systick. 
void BOARD_RunADS(const char *appName, char *boardString, char *shieldString, size_t bufferLength)
The function to register Application Name and initialte ADS. 
volatile bool bMag3110Ready
fxls8962_acceldataUser_t rawData
const registerreadlist_t cMag3110TempOut[]
Address and size of Temperature Data in Normal Mode. 
uint8_t Host_IO_Init(ARM_DRIVER_USART *pDrv, void *pBus, void *pDevInfo, void *spiSlaveParams, uint16_t slaveAddress)
This structure defines the Write command List. 
This structure defines the Read command List. 
#define MAG3110_WHOAMI_VALUE
The host_io_uart.h file contains the Host Protocol interface definitions and configuration. 
#define STREAMING_HEADER_LEN
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
int32_t MAG3110_I2C_ReadData(mag3110_i2c_sensorhandle_t *pSensorHandle, const registerreadlist_t *pReadList, uint8_t *pBuffer)
The interface function to read the sensor data. 
#define MAG3110_CTRL_REG2_AUTO_MSRT_EN_MASK
#define I2C_S_SIGNAL_EVENT
const registerreadlist_t cMag3110OutputNormal[]
Address and size of Raw Pressure+Temperature Data in Normal Mode.