![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The lpc55s69.c file defines GPIO pins and I2C CMSIS utilities for LPCXpresso55s69 board. More...
#include "lpc55s69.h"
Go to the source code of this file.
Functions | |
| void | BOARD_BootClockRUN (void) |
| Kinetis style Wrapper API for handling all Clock related configurations. More... | |
| status_t | SMC_SetPowerModeWait (void *arg) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *arg) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
| uint32_t | USART0_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | I2C4_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | SPI7_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The lpc55s69.c file defines GPIO pins and I2C CMSIS utilities for LPCXpresso55s69 board.
Definition in file lpc55s69.c.
| void BOARD_BootClockRUN | ( | void | ) |
Kinetis style Wrapper API for handling all Clock related configurations.
This function executes configuration of clocks.
| void |
Definition at line 86 of file lpc55s69.c.
References BOARD_BootClockFROHF96M().

| uint32_t I2C4_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 145 of file lpc55s69.c.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 119 of file lpc55s69.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 105 of file lpc55s69.c.
| uint32_t SPI7_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 157 of file lpc55s69.c.
| uint32_t USART0_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 133 of file lpc55s69.c.
| gpioHandleKSDK_t BLUE_LED |
Definition at line 74 of file lpc55s69.c.
Definition at line 51 of file lpc55s69.c.
Definition at line 57 of file lpc55s69.c.
| gpioHandleKSDK_t D11 |
Definition at line 31 of file lpc55s69.c.
| gpioHandleKSDK_t D12 |
Definition at line 37 of file lpc55s69.c.
| gpioHandleKSDK_t D13 |
Definition at line 43 of file lpc55s69.c.
| gpioHandleKSDK_t D14 |
Definition at line 17 of file lpc55s69.c.
| gpioHandleKSDK_t D15 |
Definition at line 23 of file lpc55s69.c.
| gpioHandleKSDK_t GREEN_LED |
Definition at line 69 of file lpc55s69.c.
| gpioHandleKSDK_t RED_LED |
Definition at line 64 of file lpc55s69.c.