22                         .clockName = kCLOCK_PortC,
    29                         .clockName = kCLOCK_PortC,
    38                        .clockName = kCLOCK_PortE,
    45                        .clockName = kCLOCK_PortE,
    54                         .clockName = kCLOCK_PortB,
    61                         .clockName = kCLOCK_PortB,
    68                         .clockName = kCLOCK_PortB,
    77                        .clockName = kCLOCK_PortA,
    84                        .clockName = kCLOCK_PortA,
    93                        .clockName = kCLOCK_PortC,
   100                        .clockName = kCLOCK_PortC,
   107                        .clockName = kCLOCK_PortB,
   114                        .clockName = kCLOCK_PortE,
   121                        .clockName = kCLOCK_PortA,
   128                        .clockName = kCLOCK_PortB,
   135                        .clockName = kCLOCK_PortB,
   142                        .clockName = kCLOCK_PortA,
   148                        .clockName = kCLOCK_PortA,
   155                        .clockName = kCLOCK_PortB,
   162                        .clockName = kCLOCK_PortB,
   169                        .clockName = kCLOCK_PortB,
   176                         .clockName = kCLOCK_PortB,
   185                             .clockName = kCLOCK_PortA,
   192                               .clockName = kCLOCK_PortA,
   199                              .clockName = kCLOCK_PortA,
   208                          .clockName = kCLOCK_PortE,
   215                          .clockName = kCLOCK_PortE,
   227     CLOCK_SetIpSrc(kCLOCK_Lpuart0, kCLOCK_IpSrcFircAsync);
   228     return CLOCK_GetIpFreq(kCLOCK_Lpuart0);
   240     CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFircAsync);
   241     return CLOCK_GetIpFreq(kCLOCK_Lpuart1);
   253     CLOCK_SetIpSrc(kCLOCK_Lpi2c0, kCLOCK_IpSrcFircAsync);
   254     return CLOCK_GetIpFreq(kCLOCK_Lpi2c0);
   266     CLOCK_SetIpSrc(kCLOCK_Lpi2c3, kCLOCK_IpSrcFircAsync);
   267     return CLOCK_GetIpFreq(kCLOCK_Lpi2c3);
   279     CLOCK_SetIpSrc(kCLOCK_Lpspi0, kCLOCK_IpSrcFircAsync);
   280     return CLOCK_GetIpFreq(kCLOCK_Lpspi0);
 
uint32_t LPUART1_GetFreq(void)
Determines the Clock Frequency feature. 
 
The GPIO pin handle for KSDK. 
 
gpioHandleKSDK_t BLUE_LED
 
uint32_t LPSPI0_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t LPI2C0_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t LPI2C3_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t LPUART0_GetFreq(void)
Determines the Clock Frequency feature. 
 
gpioHandleKSDK_t GREEN_LED
 
The frdm_k32w042.h file defines GPIO pin mappings for FRDM-K64F board.