14 #ifndef __DRIVER_GPIO_H__ 15 #define __DRIVER_GPIO_H__ 17 #include "Driver_Common.h" 19 #include "fsl_common.h" 72 #define MAKE_GPIO_HANDLE(PortName, Base, PortBase, PinNumber, Irq, ClockName, PortNumber) \ 73 static gpioHandleKSDK_t PortName##PinNumber = {.base = Base, \ 74 .portBase = PortBase, \ 75 .pinNumber = PinNumber, \ 76 .mask = 1 << (PinNumber), \ 78 .clockName = ClockName, \ 79 .portNumber = PortNumber}; 81 #define GPIO_PIN_ID(PortName, PinNumber) &(PortName##PinNumber) 84 #endif // __DRIVER_GPIO_H__ struct gpioIsrObj gpioIsrObj_t
The gpio isr object.
The GPIO Configuration KSDK.
port_number
GPIO PORT NAMES.
struct gpioHandleKSDK gpioHandleKSDK_t
The GPIO pin handle for KSDK.
void(* gpio_isr_handler_t)(void *apUserData)
Access structure of the GPIO Driver.
The Driver_GPIO.h file contains the definitions for GPIO Driver direction.
The GPIO pin handle for KSDK.
gpio_pin_config_t pinConfig
port_interrupt_t interruptMode
clock_ip_name_t clockName
struct gpioConfigKSDK gpioConfigKSDK_t
The GPIO Configuration KSDK.
enum port_number port_number_t
GPIO PORT NAMES.
port_pin_config_t portPinConfig
GENERIC_DRIVER_GPIO Driver_GPIO_KSDK