21 .clockName = kCLOCK_PortC,
28 .clockName = kCLOCK_PortC,
37 .clockName = kCLOCK_PortE,
44 .clockName = kCLOCK_PortE,
53 .clockName = kCLOCK_PortB,
60 .clockName = kCLOCK_PortB,
67 .clockName = kCLOCK_PortB,
76 .clockName = kCLOCK_PortA,
83 .clockName = kCLOCK_PortA,
92 .clockName = kCLOCK_PortC,
99 .clockName = kCLOCK_PortC,
106 .clockName = kCLOCK_PortB,
113 .clockName = kCLOCK_PortE,
120 .clockName = kCLOCK_PortA,
127 .clockName = kCLOCK_PortB,
134 .clockName = kCLOCK_PortB,
141 .clockName = kCLOCK_PortA,
147 .clockName = kCLOCK_PortA,
154 .clockName = kCLOCK_PortB,
161 .clockName = kCLOCK_PortB,
168 .clockName = kCLOCK_PortB,
175 .clockName = kCLOCK_PortB,
184 .clockName = kCLOCK_PortA,
191 .clockName = kCLOCK_PortA,
198 .clockName = kCLOCK_PortA,
207 .clockName = kCLOCK_PortE,
214 .clockName = kCLOCK_PortE,
226 CLOCK_SetIpSrc(kCLOCK_Lpuart0, kCLOCK_IpSrcFircAsync);
227 return CLOCK_GetIpFreq(kCLOCK_Lpuart0);
239 CLOCK_SetIpSrc(kCLOCK_Lpuart1, kCLOCK_IpSrcFircAsync);
240 return CLOCK_GetIpFreq(kCLOCK_Lpuart1);
252 CLOCK_SetIpSrc(kCLOCK_Lpi2c0, kCLOCK_IpSrcFircAsync);
253 return CLOCK_GetIpFreq(kCLOCK_Lpi2c0);
265 CLOCK_SetIpSrc(kCLOCK_Lpi2c3, kCLOCK_IpSrcFircAsync);
266 return CLOCK_GetIpFreq(kCLOCK_Lpi2c3);
278 CLOCK_SetIpSrc(kCLOCK_Lpspi0, kCLOCK_IpSrcFircAsync);
279 return CLOCK_GetIpFreq(kCLOCK_Lpspi0);
The GPIO pin handle for KSDK.
uint32_t LPSPI0_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t LPUART0_GetFreq(void)
Determines the Clock Frequency feature.
gpioHandleKSDK_t BLUE_LED
uint32_t LPUART1_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t LPI2C0_GetFreq(void)
Determines the Clock Frequency feature.
gpioHandleKSDK_t GREEN_LED
uint32_t LPI2C3_GetFreq(void)
Determines the Clock Frequency feature.
The frdm_k32w042.h file defines GPIO pin mappings for FRDM-K64F board.