![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The evkmimxrt1015.c file defines GPIO pins and I2C CMSIS utilities for evkmimxrt1015 board. More...
#include "evkmimxrt1015.h"
Go to the source code of this file.
Macros | |
| #define | LPI2C_CLOCK_SOURCE_SELECT (0U) |
| #define | LPI2C_CLOCK_SOURCE_DIVIDER (5U) |
| #define | LPI2C_CLOCK_FREQUENCY ((CLOCK_GetFreq(kCLOCK_Usb1PllClk) / 8) / (LPI2C_CLOCK_SOURCE_DIVIDER + 1U)) |
Functions | |
| status_t | SMC_SetPowerModeWait (void *arg) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *arg) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
| uint32_t | LPUART1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | LPI2C1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | LPSPI1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The evkmimxrt1015.c file defines GPIO pins and I2C CMSIS utilities for evkmimxrt1015 board.
Definition in file evkmimxrt1015.c.
| #define LPI2C_CLOCK_FREQUENCY ((CLOCK_GetFreq(kCLOCK_Usb1PllClk) / 8) / (LPI2C_CLOCK_SOURCE_DIVIDER + 1U)) |
Definition at line 23 of file evkmimxrt1015.c.
| #define LPI2C_CLOCK_SOURCE_DIVIDER (5U) |
Definition at line 21 of file evkmimxrt1015.c.
Referenced by LPI2C1_GetFreq().
| #define LPI2C_CLOCK_SOURCE_SELECT (0U) |
Definition at line 19 of file evkmimxrt1015.c.
Referenced by LPI2C1_GetFreq().
| uint32_t LPI2C1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 162 of file evkmimxrt1015.c.
References LPI2C_CLOCK_SOURCE_DIVIDER, and LPI2C_CLOCK_SOURCE_SELECT.
| uint32_t LPSPI1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 177 of file evkmimxrt1015.c.
| uint32_t LPUART1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 150 of file evkmimxrt1015.c.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 135 of file evkmimxrt1015.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 120 of file evkmimxrt1015.c.
Definition at line 64 of file evkmimxrt1015.c.
Definition at line 66 of file evkmimxrt1015.c.
Definition at line 68 of file evkmimxrt1015.c.
Definition at line 70 of file evkmimxrt1015.c.
Definition at line 38 of file evkmimxrt1015.c.
Definition at line 35 of file evkmimxrt1015.c.
| gpioHandleiMXSDK_t BLUE_LED |
Definition at line 95 of file evkmimxrt1015.c.
Definition at line 57 of file evkmimxrt1015.c.
Definition at line 60 of file evkmimxrt1015.c.
Definition at line 52 of file evkmimxrt1015.c.
Definition at line 49 of file evkmimxrt1015.c.
Definition at line 46 of file evkmimxrt1015.c.
Definition at line 43 of file evkmimxrt1015.c.
Definition at line 30 of file evkmimxrt1015.c.
Definition at line 27 of file evkmimxrt1015.c.
Definition at line 72 of file evkmimxrt1015.c.
Definition at line 74 of file evkmimxrt1015.c.
Definition at line 76 of file evkmimxrt1015.c.
Definition at line 78 of file evkmimxrt1015.c.
Definition at line 80 of file evkmimxrt1015.c.
Definition at line 82 of file evkmimxrt1015.c.
Definition at line 84 of file evkmimxrt1015.c.
Definition at line 86 of file evkmimxrt1015.c.
| gpioHandleiMXSDK_t GREEN_LED |
Definition at line 93 of file evkmimxrt1015.c.
| gpioHandleiMXSDK_t INT1 |
Definition at line 99 of file evkmimxrt1015.c.
| gpioHandleiMXSDK_t INT2 |
Definition at line 101 of file evkmimxrt1015.c.
| gpioHandleiMXSDK_t RED_LED |
Definition at line 91 of file evkmimxrt1015.c.