![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The evkmimxrt1020.c file defines GPIO pins and I2C CMSIS utilities for evkmimxrt1020 board. More...
#include "evkmimxrt1020.h"
Go to the source code of this file.
Functions | |
| status_t | SMC_SetPowerModeWait (void *arg) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *arg) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
| uint32_t | LPUART1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | LPI2C1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | LPSPI1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The evkmimxrt1020.c file defines GPIO pins and I2C CMSIS utilities for evkmimxrt1020 board.
Definition in file evkmimxrt1020.c.
| uint32_t LPI2C1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 234 of file evkmimxrt1020.c.
| uint32_t LPSPI1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 246 of file evkmimxrt1020.c.
| uint32_t LPUART1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 222 of file evkmimxrt1020.c.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 207 of file evkmimxrt1020.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 192 of file evkmimxrt1020.c.
Definition at line 84 of file evkmimxrt1020.c.
Definition at line 89 of file evkmimxrt1020.c.
Definition at line 94 of file evkmimxrt1020.c.
Definition at line 99 of file evkmimxrt1020.c.
Definition at line 37 of file evkmimxrt1020.c.
Definition at line 31 of file evkmimxrt1020.c.
| gpioHandleiMXSDK_t BLUE_LED |
Definition at line 157 of file evkmimxrt1020.c.
Definition at line 71 of file evkmimxrt1020.c.
Definition at line 77 of file evkmimxrt1020.c.
Definition at line 63 of file evkmimxrt1020.c.
Definition at line 57 of file evkmimxrt1020.c.
Definition at line 51 of file evkmimxrt1020.c.
Definition at line 45 of file evkmimxrt1020.c.
Definition at line 23 of file evkmimxrt1020.c.
Definition at line 17 of file evkmimxrt1020.c.
Definition at line 104 of file evkmimxrt1020.c.
Definition at line 109 of file evkmimxrt1020.c.
Definition at line 114 of file evkmimxrt1020.c.
Definition at line 119 of file evkmimxrt1020.c.
Definition at line 124 of file evkmimxrt1020.c.
Definition at line 129 of file evkmimxrt1020.c.
Definition at line 134 of file evkmimxrt1020.c.
Definition at line 139 of file evkmimxrt1020.c.
| gpioHandleiMXSDK_t GREEN_LED |
Definition at line 152 of file evkmimxrt1020.c.
| gpioHandleiMXSDK_t INT1 |
Definition at line 164 of file evkmimxrt1020.c.
| gpioHandleiMXSDK_t INT2 |
Definition at line 169 of file evkmimxrt1020.c.
| gpioHandleiMXSDK_t RED_LED |
Definition at line 147 of file evkmimxrt1020.c.