20 .irq = GPIO1_Combined_0_15_IRQn,
26 .irq = GPIO1_Combined_0_15_IRQn,
34 .irq = GPIO1_Combined_0_15_IRQn,
40 .irq = GPIO1_Combined_0_15_IRQn,
48 .irq = GPIO3_Combined_0_15_IRQn,
54 .irq = GPIO3_Combined_0_15_IRQn,
60 .irq = GPIO3_Combined_0_15_IRQn,
66 .irq = GPIO3_Combined_0_15_IRQn,
74 .irq = GPIO2_Combined_0_15_IRQn,
80 .irq = GPIO2_Combined_16_31_IRQn,
87 .irq = GPIO1_Combined_16_31_IRQn,
92 .irq = GPIO1_Combined_16_31_IRQn,
97 .irq = GPIO1_Combined_16_31_IRQn,
102 .irq = GPIO1_Combined_16_31_IRQn,
107 .irq = GPIO1_Combined_0_15_IRQn,
112 .irq = GPIO1_Combined_16_31_IRQn,
117 .irq = GPIO1_Combined_0_15_IRQn,
122 .irq = GPIO1_Combined_0_15_IRQn,
127 .irq = GPIO1_Combined_16_31_IRQn,
132 .irq = GPIO1_Combined_16_31_IRQn,
137 .irq = GPIO1_Combined_0_15_IRQn,
142 .irq = GPIO1_Combined_0_15_IRQn,
150 .irq = GPIO1_Combined_0_15_IRQn,
155 .irq = GPIO1_Combined_0_15_IRQn,
160 .irq = GPIO1_Combined_0_15_IRQn,
167 .irq = GPIO1_Combined_0_15_IRQn,
172 .irq = GPIO1_Combined_0_15_IRQn,
179 static void stop(
void)
181 SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
194 CLOCK_SetMode(kCLOCK_ModeWait);
197 return kStatus_Success;
209 CLOCK_SetMode(kCLOCK_ModeWait);
212 return kStatus_Success;
224 return CLOCK_GetFreq((clock_name_t) kCLOCK_Lpuart1);
236 return CLOCK_GetFreq((clock_name_t) kCLOCK_Lpi2c1);
248 return CLOCK_GetFreq((clock_name_t) kCLOCK_Lpspi1);
gpioHandleiMXSDK_t BLUE_LED
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
gpioHandleiMXSDK_t GREEN_LED
uint32_t LPI2C1_GetFreq(void)
Determines the Clock Frequency feature.
uint32_t LPSPI1_GetFreq(void)
Determines the Clock Frequency feature.
gpioHandleiMXSDK_t RED_LED
uint32_t LPUART1_GetFreq(void)
Determines the Clock Frequency feature.
The GPIO pin handle for i.MX SDK.
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
The evkmimxrt1020.h file defines GPIO pin mappings for evkmimxrt1020 board.