![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The evkmimxrt1024.c file defines GPIO pins and I2C CMSIS utilities for evkmimxrt1024 board. More...
#include "evkmimxrt1024.h"
Go to the source code of this file.
Functions | |
| status_t | SMC_SetPowerModeWait (void *arg) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *arg) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
| uint32_t | LPUART1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | LPI2C1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
| uint32_t | LPSPI1_GetFreq (void) |
| Determines the Clock Frequency feature. More... | |
The evkmimxrt1024.c file defines GPIO pins and I2C CMSIS utilities for evkmimxrt1024 board.
Definition in file evkmimxrt1024.c.
| uint32_t LPI2C1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_i2c_cmsis.c.
| [in] | void |
Definition at line 152 of file evkmimxrt1024.c.
References LPI2C_CLOCK_FREQUENCY.
| uint32_t LPSPI1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_spi_cmsis.c.
| [in] | void |
Definition at line 164 of file evkmimxrt1024.c.
References LPSPI_CLOCK_FREQUENCY.
| uint32_t LPUART1_GetFreq | ( | void | ) |
Determines the Clock Frequency feature.
The Clock Frequecny computation API required by fsl_uart_cmsis.c.
| [in] | void |
Definition at line 140 of file evkmimxrt1024.c.
References BOARD_DebugConsoleSrcFreq().

| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 125 of file evkmimxrt1024.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 110 of file evkmimxrt1024.c.
Definition at line 54 of file evkmimxrt1024.c.
Definition at line 56 of file evkmimxrt1024.c.
Definition at line 58 of file evkmimxrt1024.c.
Definition at line 60 of file evkmimxrt1024.c.
Definition at line 28 of file evkmimxrt1024.c.
Definition at line 25 of file evkmimxrt1024.c.
| gpioHandleiMXSDK_t BLUE_LED |
Definition at line 85 of file evkmimxrt1024.c.
Definition at line 47 of file evkmimxrt1024.c.
Definition at line 50 of file evkmimxrt1024.c.
Definition at line 42 of file evkmimxrt1024.c.
Definition at line 39 of file evkmimxrt1024.c.
Definition at line 36 of file evkmimxrt1024.c.
Definition at line 33 of file evkmimxrt1024.c.
Definition at line 20 of file evkmimxrt1024.c.
Definition at line 17 of file evkmimxrt1024.c.
Definition at line 62 of file evkmimxrt1024.c.
Definition at line 64 of file evkmimxrt1024.c.
Definition at line 66 of file evkmimxrt1024.c.
Definition at line 68 of file evkmimxrt1024.c.
Definition at line 70 of file evkmimxrt1024.c.
Definition at line 72 of file evkmimxrt1024.c.
Definition at line 74 of file evkmimxrt1024.c.
Definition at line 76 of file evkmimxrt1024.c.
| gpioHandleiMXSDK_t GREEN_LED |
Definition at line 83 of file evkmimxrt1024.c.
| gpioHandleiMXSDK_t INT1 |
Definition at line 89 of file evkmimxrt1024.c.
| gpioHandleiMXSDK_t INT2 |
Definition at line 91 of file evkmimxrt1024.c.
| gpioHandleiMXSDK_t RED_LED |
Definition at line 81 of file evkmimxrt1024.c.