18     .
base = GPIO1, .pinNumber = 2, .mask = 1 << (2), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    21     .
base = GPIO1, .pinNumber = 3, .mask = 1 << (3), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    26     .
base = GPIO1, .pinNumber = 14, .mask = 1 << (14), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    29     .
base = GPIO1, .pinNumber = 15, .mask = 1 << (15), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    34     .
base = GPIO3, .pinNumber = 10, .mask = 1 << (10), .irq = GPIO3_Combined_0_15_IRQn, .portNumber = 
GPIO3_NUM};
    37     .
base = GPIO3, .pinNumber = 13, .mask = 1 << (13), .irq = GPIO3_Combined_0_15_IRQn, .portNumber = 
GPIO3_NUM};
    40     .
base = GPIO3, .pinNumber = 12, .mask = 1 << (12), .irq = GPIO3_Combined_0_15_IRQn, .portNumber = 
GPIO3_NUM};
    43     .
base = GPIO3, .pinNumber = 11, .mask = 1 << (11), .irq = GPIO3_Combined_0_15_IRQn, .portNumber = 
GPIO3_NUM};
    48     .
base = GPIO2, .pinNumber = 9, .mask = 1 << (9), .irq = GPIO2_Combined_0_15_IRQn, .portNumber = 
GPIO2_NUM};
    51     .
base = GPIO2, .pinNumber = 8, .mask = 1 << (8), .irq = GPIO2_Combined_16_31_IRQn, .portNumber = 
GPIO2_NUM};
    55     .
base = GPIO1, .pinNumber = 26, .mask = 1 << (26), .irq = GPIO1_Combined_16_31_IRQn, .portNumber = 
GPIO1_NUM};
    57     .
base = GPIO1, .pinNumber = 27, .mask = 1 << (27), .irq = GPIO1_Combined_16_31_IRQn, .portNumber = 
GPIO1_NUM};
    59     .
base = GPIO1, .pinNumber = 20, .mask = 1 << (20), .irq = GPIO1_Combined_16_31_IRQn, .portNumber = 
GPIO1_NUM};
    61     .
base = GPIO1, .pinNumber = 21, .mask = 1 << (21), .irq = GPIO1_Combined_16_31_IRQn, .portNumber = 
GPIO1_NUM};
    63     .
base = GPIO1, .pinNumber = 11, .mask = 1 << (11), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    65     .
base = GPIO1, .pinNumber = 24, .mask = 1 << (24), .irq = GPIO1_Combined_16_31_IRQn, .portNumber = 
GPIO1_NUM};
    67     .
base = GPIO1, .pinNumber = 9, .mask = 1 << (9), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    69     .
base = GPIO1, .pinNumber = 10, .mask = 1 << (10), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    71     .
base = GPIO1, .pinNumber = 18, .mask = 1 << (18), .irq = GPIO1_Combined_16_31_IRQn, .portNumber = 
GPIO1_NUM};
    73     .
base = GPIO1, .pinNumber = 19, .mask = 1 << (19), .irq = GPIO1_Combined_16_31_IRQn, .portNumber = 
GPIO1_NUM};
    75     .
base = GPIO1, .pinNumber = 3, .mask = 1 << (3), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    77     .
base = GPIO1, .pinNumber = 2, .mask = 1 << (2), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    82     .
base = GPIO1, .pinNumber = 9, .mask = 1 << (9), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    84     .
base = GPIO1, .pinNumber = 9, .mask = 1 << (9), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    86     .
base = GPIO1, .pinNumber = 9, .mask = 1 << (9), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    90     .
base = GPIO1, .pinNumber = 10, .mask = 1 << (10), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    92     .
base = GPIO1, .pinNumber = 11, .mask = 1 << (11), .irq = GPIO1_Combined_0_15_IRQn, .portNumber = 
GPIO1_NUM};
    97 static void stop(
void)
    99     SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
   112     CLOCK_SetMode(kCLOCK_ModeWait);
   115     return kStatus_Success;
   127     CLOCK_SetMode(kCLOCK_ModeWait);
   130     return kStatus_Success;
 The evkmimxrt1024.h file defines GPIO pin mappings for evkmimxrt1024 board. 
 
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
 
uint32_t LPI2C1_GetFreq(void)
Determines the Clock Frequency feature. 
 
uint32_t BOARD_DebugConsoleSrcFreq(void)
 
uint32_t LPUART1_GetFreq(void)
Determines the Clock Frequency feature. 
 
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
 
gpioHandleiMXSDK_t BLUE_LED
 
#define LPI2C_CLOCK_FREQUENCY
 
gpioHandleiMXSDK_t RED_LED
 
gpioHandleiMXSDK_t GREEN_LED
 
uint32_t LPSPI1_GetFreq(void)
Determines the Clock Frequency feature. 
 
The GPIO pin handle for i.MX SDK. 
 
#define LPSPI_CLOCK_FREQUENCY