18 static void stop(
void)
20 SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
33 CLOCK_SetMode(kCLOCK_ModeWait);
36 return kStatus_Success;
48 CLOCK_SetMode(kCLOCK_ModeWait);
51 return kStatus_Success;
75 return CLOCK_GetFreq(kCLOCK_OscRc48MDiv2);
87 return CLOCK_GetFreqFromObs(CCM_OBS_LPSPI1_CLK_ROOT);
uint32_t BOARD_DebugConsoleSrcFreq(void)
uint32_t LPSPI1_GetFreq(void)
Determines the Clock Frequency feature.
status_t SMC_SetPowerModeWait(void *arg)
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility...
uint32_t LPI2C1_GetFreq(void)
Determines the Clock Frequency feature.
The evkmimxrt1170.h file defines GPIO pin mappings for evkmimxrt1170 board.
status_t SMC_SetPowerModeVlpr(void *arg)
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility...
uint32_t LPUART1_GetFreq(void)
Determines the Clock Frequency feature.