![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
The evkmimxrt1170.h file defines GPIO pin mappings for evkmimxrt1170 board. More...
#include "pin_mux.h"#include "board.h"#include "RTE_Device.h"#include "gpio_driver.h"#include "MIMXRT1176_cm7.h"

Go to the source code of this file.
Macros | |
| #define | I2C_S1_SCL_PIN IOMUXC_GPIO_LPSR_05_LPI2C5_SCL |
| #define | I2C_S1_SDA_PIN IOMUXC_GPIO_LPSR_04_LPI2C5_SDA |
| #define | I2C_S1_DRIVER Driver_I2C5 |
| #define | I2C_S1_DEVICE_INDEX I2C5_INDEX |
| #define | I2C_S1_SIGNAL_EVENT I2C5_SignalEvent_t |
| #define | I2C_S2_SCL_PIN IOMUXC_GPIO_AD_08_LPI2C1_SCL |
| #define | I2C_S2_SDA_PIN IOMUXC_GPIO_AD_09_LPI2C1_SDA |
| #define | I2C_S2_DRIVER Driver_I2C1 |
| #define | I2C_S2_DEVICE_INDEX I2C1_INDEX |
| #define | I2C_S2_SIGNAL_EVENT I2C1_SignalEvent_t |
| #define | HOST_S_DRIVER Driver_USART1 |
| #define | HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
| #define | ASK_USER_TO_RESUME(x) |
| #define | I2C1 LPI2C1 |
| #define | I2C_Type LPI2C_Type |
| #define | I2C_BASE_PTRS LPI2C_BASE_PTRS |
| #define | SPI1 LPSPI1 |
| #define | SPI_Type LPSPI_Type |
| #define | SPI_BASE_PTRS LPSPI_BASE_PTRS |
| #define | SMC NULL |
Functions | |
| status_t | SMC_SetPowerModeWait (void *) |
| Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility. More... | |
| status_t | SMC_SetPowerModeVlpr (void *) |
| Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility. More... | |
The evkmimxrt1170.h file defines GPIO pin mappings for evkmimxrt1170 board.
Definition in file evkmimxrt1170.h.
| #define ASK_USER_TO_RESUME | ( | x | ) |
Definition at line 43 of file evkmimxrt1170.h.
| #define HOST_S_DRIVER Driver_USART1 |
Definition at line 39 of file evkmimxrt1170.h.
| #define HOST_S_SIGNAL_EVENT HOST_SignalEvent_t |
Definition at line 40 of file evkmimxrt1170.h.
| #define I2C1 LPI2C1 |
Definition at line 54 of file evkmimxrt1170.h.
| #define I2C_BASE_PTRS LPI2C_BASE_PTRS |
Definition at line 56 of file evkmimxrt1170.h.
| #define I2C_S1_DEVICE_INDEX I2C5_INDEX |
Definition at line 28 of file evkmimxrt1170.h.
| #define I2C_S1_DRIVER Driver_I2C5 |
Definition at line 27 of file evkmimxrt1170.h.
| #define I2C_S1_SCL_PIN IOMUXC_GPIO_LPSR_05_LPI2C5_SCL |
Definition at line 25 of file evkmimxrt1170.h.
| #define I2C_S1_SDA_PIN IOMUXC_GPIO_LPSR_04_LPI2C5_SDA |
Definition at line 26 of file evkmimxrt1170.h.
| #define I2C_S1_SIGNAL_EVENT I2C5_SignalEvent_t |
Definition at line 29 of file evkmimxrt1170.h.
| #define I2C_S2_DEVICE_INDEX I2C1_INDEX |
Definition at line 35 of file evkmimxrt1170.h.
| #define I2C_S2_DRIVER Driver_I2C1 |
Definition at line 34 of file evkmimxrt1170.h.
| #define I2C_S2_SCL_PIN IOMUXC_GPIO_AD_08_LPI2C1_SCL |
Definition at line 32 of file evkmimxrt1170.h.
| #define I2C_S2_SDA_PIN IOMUXC_GPIO_AD_09_LPI2C1_SDA |
Definition at line 33 of file evkmimxrt1170.h.
| #define I2C_S2_SIGNAL_EVENT I2C1_SignalEvent_t |
Definition at line 36 of file evkmimxrt1170.h.
| #define I2C_Type LPI2C_Type |
Definition at line 55 of file evkmimxrt1170.h.
| #define SMC NULL |
Definition at line 62 of file evkmimxrt1170.h.
| #define SPI1 LPSPI1 |
Definition at line 57 of file evkmimxrt1170.h.
| #define SPI_BASE_PTRS LPSPI_BASE_PTRS |
Definition at line 59 of file evkmimxrt1170.h.
| #define SPI_Type LPSPI_Type |
Definition at line 58 of file evkmimxrt1170.h.
| status_t SMC_SetPowerModeVlpr | ( | void * | arg | ) |
Configures the system to VLPR power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 169 of file lpc54114.c.
| status_t SMC_SetPowerModeWait | ( | void * | arg | ) |
Configures the system to WAIT power mode. API name used from Kinetis family to maintain compatibility.
| Power | peripheral base address (dummy). |
Definition at line 155 of file lpc54114.c.