![]() |
ISSDK
1.8
IoT Sensing Software Development Kit
|
A "standard" build configuration file. More...
Go to the source code of this file.
Macros | |
| #define | THISBUILD 700 |
| define build number sent in debug packet for display purposes only More... | |
CoordinateSystemBitFields | |
These defines determine the frame of reference (x, y, z axes and Euler angles) standard to be used for a particular build. Change THISCOORDSYSTEM to whichever of NED, ANDROID or WIN8 you prefer. | |
| #define | NED 0 |
| identifier for NED (Aerospace) axes and angles More... | |
| #define | ANDROID 1 |
| identifier for Android axes and angles More... | |
| #define | WIN8 2 |
| identifier for Windows 8 axes and angles More... | |
| #define | THISCOORDSYSTEM NED |
| the coordinate system to be used More... | |
SensorBitFields | |
These bit-field values are used to declare which sensor types are used in the application. Change bit-field values to 0x0000 for any features NOT USED | |
| #define | F_USING_ACCEL 0x0001 |
| nominally 0x0001 if an accelerometer is to be used, 0x0000 otherwise More... | |
| #define | F_USING_MAG 0x0002 |
| nominally 0x0002 if an magnetometer is to be used, 0x0000 otherwise More... | |
| #define | F_USING_GYRO 0x0004 |
| nominally 0x0004 if a gyro is to be used, 0x0000 otherwise More... | |
| #define | F_USING_PRESSURE 0x0008 |
| nominally 0x0008 if altimeter is to be used, 0x0000 otherwise More... | |
| #define | F_USING_TEMPERATURE 0x0010 |
| nominally 0x0010 if temp sensor is to be used, 0x0000 otherwise More... | |
| #define | F_ALL_SENSORS 0x001F |
| refers to all applicable sensor types for the given physical unit More... | |
FusionSelectionBitFields | |
These bit-field values are used to declare which sensor fusion algorithms are used in the application. You can use more than one, altough they all run from the same data. Change individual bit-field values to 0x0000 for any features NOT USED. | |
| #define | F_1DOF_P_BASIC 0x0100 |
| 1DOF pressure (altitude) and temperature algorithm selector - 0x0100 to include, 0x0000 otherwise More... | |
| #define | F_3DOF_G_BASIC 0x0200 |
| 3DOF accel tilt (accel) algorithm selector - 0x0200 to include, 0x0000 otherwise More... | |
| #define | F_3DOF_B_BASIC 0x0400 |
| 3DOF mag eCompass (vehicle/mag) algorithm selector - 0x0400 to include, 0x0000 otherwise More... | |
| #define | F_3DOF_Y_BASIC 0x0800 |
| 3DOF gyro integration algorithm selector - 0x0800 to include, 0x0000 otherwise More... | |
| #define | F_6DOF_GB_BASIC 0x1000 |
| 6DOF accel and mag eCompass algorithm selector - 0x1000 to include, 0x0000 otherwise More... | |
| #define | F_6DOF_GY_KALMAN 0x2000 |
| 6DOF accel and gyro (Kalman) algorithm selector - 0x2000 to include, 0x0000 otherwise More... | |
| #define | F_9DOF_GBY_KALMAN 0x4000 |
| 9DOF accel, mag and gyro algorithm selector - 0x4000 to include, 0x0000 otherwise More... | |
SensorParameters | |
FIFO sizes effect the size of the sensor data structures. ODR refers to "Output Data Rate" | |
| #define | ACCEL_FIFO_SIZE 32 |
| FXOS8700 (accel), MMA8652, FXLS8952 all have 32 element FIFO. More... | |
| #define | MAG_FIFO_SIZE 16 |
| FXOS8700 (mag), MAG3110 have no FIFO so equivalent to 1 element FIFO. More... | |
| #define | GYRO_FIFO_SIZE 32 |
| FXAX21000, FXAS21002 have 32 element FIFO. More... | |
| #define | ACCEL_ODR_HZ 200 |
| (int) requested accelerometer ODR Hz (over-rides MAG_ODR_HZ for FXOS8700) More... | |
| #define | MAG_ODR_HZ 200 |
| (int) requested magnetometer ODR Hz (over-ridden by ACCEL_ODR_HZ for FXOS8700) More... | |
| #define | GYRO_ODR_HZ 400 |
| (int) requested gyroscope ODR Hz More... | |
| #define | FUSION_HZ 40 |
| (int) actual rate of fusion algorithm execution and sensor FIFO reads More... | |
| #define | FAST_LOOP_HZ 80 |
| Over Sample Ratio * FUSION_HZ when using no FIFO. More... | |
| #define | OVERSAMPLE_RATE FAST_LOOP_HZ/FUSION_HZ |
A "standard" build configuration file.
This file contains only those parameters that directly relate to fusion implementation choices. Board dependencies are in hal_<shield_board>.h. Consult the Sensor Fusion User Guide for guidance and details.
Definition in file standard_build.h.
| #define ACCEL_FIFO_SIZE 32 |
FXOS8700 (accel), MMA8652, FXLS8952 all have 32 element FIFO.
Definition at line 62 of file standard_build.h.
Referenced by FXLS8471Q_Read(), and FXOS8700_Init().
| #define ACCEL_ODR_HZ 200 |
(int) requested accelerometer ODR Hz (over-rides MAG_ODR_HZ for FXOS8700)
Definition at line 65 of file standard_build.h.
| #define ANDROID 1 |
identifier for Android axes and angles
Definition at line 29 of file standard_build.h.
| #define F_1DOF_P_BASIC 0x0100 |
1DOF pressure (altitude) and temperature algorithm selector - 0x0100 to include, 0x0000 otherwise
Definition at line 50 of file standard_build.h.
Referenced by CreateAndSendPackets(), and initSensorFusionGlobals().
| #define F_3DOF_B_BASIC 0x0400 |
3DOF mag eCompass (vehicle/mag) algorithm selector - 0x0400 to include, 0x0000 otherwise
Definition at line 52 of file standard_build.h.
Referenced by CreateAndSendPackets(), initializeFusionEngine(), and initSensorFusionGlobals().
| #define F_3DOF_G_BASIC 0x0200 |
3DOF accel tilt (accel) algorithm selector - 0x0200 to include, 0x0000 otherwise
Definition at line 51 of file standard_build.h.
Referenced by CreateAndSendPackets(), and initSensorFusionGlobals().
| #define F_3DOF_Y_BASIC 0x0800 |
3DOF gyro integration algorithm selector - 0x0800 to include, 0x0000 otherwise
Definition at line 53 of file standard_build.h.
Referenced by CreateAndSendPackets(), initializeFusionEngine(), and initSensorFusionGlobals().
| #define F_6DOF_GB_BASIC 0x1000 |
6DOF accel and mag eCompass algorithm selector - 0x1000 to include, 0x0000 otherwise
Definition at line 54 of file standard_build.h.
Referenced by CreateAndSendPackets(), initializeFusionEngine(), and initSensorFusionGlobals().
| #define F_6DOF_GY_KALMAN 0x2000 |
6DOF accel and gyro (Kalman) algorithm selector - 0x2000 to include, 0x0000 otherwise
Definition at line 55 of file standard_build.h.
Referenced by CreateAndSendPackets(), initializeFusionEngine(), initSensorFusionGlobals(), and SaveGyroCalibrationToNVM().
| #define F_9DOF_GBY_KALMAN 0x4000 |
9DOF accel, mag and gyro algorithm selector - 0x4000 to include, 0x0000 otherwise
Definition at line 56 of file standard_build.h.
Referenced by CreateAndSendPackets(), initializeFusionEngine(), and initSensorFusionGlobals().
| #define F_ALL_SENSORS 0x001F |
refers to all applicable sensor types for the given physical unit
Definition at line 43 of file standard_build.h.
Referenced by initSensorFusionGlobals().
| #define F_USING_ACCEL 0x0001 |
nominally 0x0001 if an accelerometer is to be used, 0x0000 otherwise
Definition at line 38 of file standard_build.h.
Referenced by CreateAndSendPackets(), FXLS8471Q_Idle(), FXLS8471Q_Init(), FXLS8471Q_Read(), FXOS8700_Idle(), FXOS8700_Init(), and initSensorFusionGlobals().
| #define F_USING_GYRO 0x0004 |
nominally 0x0004 if a gyro is to be used, 0x0000 otherwise
Definition at line 40 of file standard_build.h.
Referenced by CreateAndSendPackets(), and initSensorFusionGlobals().
| #define F_USING_MAG 0x0002 |
nominally 0x0002 if an magnetometer is to be used, 0x0000 otherwise
Definition at line 39 of file standard_build.h.
| #define F_USING_PRESSURE 0x0008 |
nominally 0x0008 if altimeter is to be used, 0x0000 otherwise
Definition at line 41 of file standard_build.h.
Referenced by initSensorFusionGlobals().
| #define F_USING_TEMPERATURE 0x0010 |
nominally 0x0010 if temp sensor is to be used, 0x0000 otherwise
Definition at line 42 of file standard_build.h.
Referenced by initSensorFusionGlobals().
| #define FAST_LOOP_HZ 80 |
Over Sample Ratio * FUSION_HZ when using no FIFO.
Definition at line 69 of file standard_build.h.
| #define FUSION_HZ 40 |
(int) actual rate of fusion algorithm execution and sensor FIFO reads
Definition at line 68 of file standard_build.h.
Referenced by CreateAndSendPackets(), DecodeCommandBytes(), fInit_1DOF_P_BASIC(), fInit_3DOF_B_BASIC(), fInit_3DOF_G_BASIC(), fInit_3DOF_Y_BASIC(), fInit_6DOF_GB_BASIC(), fInit_6DOF_GY_KALMAN(), fInit_9DOF_GBY_KALMAN(), fRunMagCalibration(), fUpdateAccelBuffer(), main(), and throttle().
| #define GYRO_FIFO_SIZE 32 |
FXAX21000, FXAS21002 have 32 element FIFO.
Definition at line 64 of file standard_build.h.
| #define GYRO_ODR_HZ 400 |
(int) requested gyroscope ODR Hz
Definition at line 67 of file standard_build.h.
| #define MAG_FIFO_SIZE 16 |
FXOS8700 (mag), MAG3110 have no FIFO so equivalent to 1 element FIFO.
Definition at line 63 of file standard_build.h.
Referenced by FXOS8700_ReadMagData(), and MAG3110_Read().
| #define MAG_ODR_HZ 200 |
(int) requested magnetometer ODR Hz (over-ridden by ACCEL_ODR_HZ for FXOS8700)
Definition at line 66 of file standard_build.h.
| #define NED 0 |
identifier for NED (Aerospace) axes and angles
Definition at line 28 of file standard_build.h.
| #define OVERSAMPLE_RATE FAST_LOOP_HZ/FUSION_HZ |
Definition at line 70 of file standard_build.h.
| #define THISBUILD 700 |
define build number sent in debug packet for display purposes only
Definition at line 21 of file standard_build.h.
Referenced by CreateAndSendPackets().
| #define THISCOORDSYSTEM NED |
the coordinate system to be used
Definition at line 31 of file standard_build.h.
| #define WIN8 2 |
identifier for Windows 8 axes and angles
Definition at line 30 of file standard_build.h.