ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_DEVSTAT_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_DEVSTAT_t:
Collaboration graph

Data Fields

struct {
   uint8_t   devinit: 1
 
   uint8_t   devres: 1
 
   uint8_t   testmode: 1
 
   uint8_t   supply_err: 1
 
   uint8_t   memtemp_err: 1
 
   uint8_t   comm_err: 1
 
   uint8_t   _reserved_: 1
 
   uint8_t   dsp_err: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 155 of file dbap.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 163 of file dbap.h.

◆ b

struct { ... } b

◆ comm_err

uint8_t comm_err

Definition at line 162 of file dbap.h.

◆ devinit

uint8_t devinit

Definition at line 157 of file dbap.h.

◆ devres

uint8_t devres

Definition at line 158 of file dbap.h.

◆ dsp_err

uint8_t dsp_err

Definition at line 164 of file dbap.h.

◆ memtemp_err

uint8_t memtemp_err

Definition at line 161 of file dbap.h.

◆ supply_err

uint8_t supply_err

Definition at line 160 of file dbap.h.

◆ testmode

uint8_t testmode

Definition at line 159 of file dbap.h.

◆ w

uint8_t w

Definition at line 166 of file dbap.h.


The documentation for this union was generated from the following file: