ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_DEVSTAT1_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_DEVSTAT1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   cont_err: 1
 
   uint8_t   intregf_err: 1
 
   uint8_t   intreg_err: 1
 
   uint8_t   intrega_err: 1
 
   uint8_t   _reserved1_: 1
 
   uint8_t   vccov_err: 1
 
   uint8_t   _reserved2_: 1
 
   uint8_t   vccuv_err: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 218 of file dbap.h.

Field Documentation

◆ _reserved1_

uint8_t _reserved1_

Definition at line 224 of file dbap.h.

◆ _reserved2_

uint8_t _reserved2_

Definition at line 226 of file dbap.h.

◆ b

struct { ... } b

◆ cont_err

uint8_t cont_err

Definition at line 220 of file dbap.h.

◆ intreg_err

uint8_t intreg_err

Definition at line 222 of file dbap.h.

◆ intrega_err

uint8_t intrega_err

Definition at line 223 of file dbap.h.

◆ intregf_err

uint8_t intregf_err

Definition at line 221 of file dbap.h.

◆ vccov_err

uint8_t vccov_err

Definition at line 225 of file dbap.h.

◆ vccuv_err

uint8_t vccuv_err

Definition at line 227 of file dbap.h.

◆ w

uint8_t w

Definition at line 230 of file dbap.h.


The documentation for this union was generated from the following file: