ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_DEVSTAT2_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_DEVSTAT2_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved1_: 2
 
   uint8_t   temp0_err: 1
 
   uint8_t   _reserved2_: 1
 
   uint8_t   u_w_active: 1
 
   uint8_t   u_rw_err: 1
 
   uint8_t   u_otp_err: 1
 
   uint8_t   f_otp_err: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 278 of file dbap.h.

Field Documentation

◆ _reserved1_

uint8_t _reserved1_

Definition at line 280 of file dbap.h.

◆ _reserved2_

uint8_t _reserved2_

Definition at line 282 of file dbap.h.

◆ b

struct { ... } b

◆ f_otp_err

uint8_t f_otp_err

Definition at line 286 of file dbap.h.

◆ temp0_err

uint8_t temp0_err

Definition at line 281 of file dbap.h.

◆ u_otp_err

uint8_t u_otp_err

Definition at line 285 of file dbap.h.

◆ u_rw_err

uint8_t u_rw_err

Definition at line 284 of file dbap.h.

◆ u_w_active

uint8_t u_w_active

Definition at line 283 of file dbap.h.

◆ w

uint8_t w

Definition at line 289 of file dbap.h.


The documentation for this union was generated from the following file: