ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_DEVSTAT3_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_DEVSTAT3_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 6
 
   uint8_t   osctrain_err: 1
 
   uint8_t   miso_err: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 334 of file dbap.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 336 of file dbap.h.

◆ b

struct { ... } b

◆ miso_err

uint8_t miso_err

Definition at line 338 of file dbap.h.

◆ osctrain_err

uint8_t osctrain_err

Definition at line 337 of file dbap.h.

◆ w

uint8_t w

Definition at line 341 of file dbap.h.


The documentation for this union was generated from the following file: