ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_DEVLOCK_WR_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_DEVLOCK_WR_t:
Collaboration graph

Data Fields

struct {
   uint8_t   reset: 2
 
   uint8_t   _reserved1_: 1
 
   uint8_t   sup_err_dis: 1
 
   uint8_t   _reserved2_: 3
 
   uint8_t   endinit: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 383 of file dbap.h.

Field Documentation

◆ _reserved1_

uint8_t _reserved1_

Definition at line 386 of file dbap.h.

◆ _reserved2_

uint8_t _reserved2_

Definition at line 388 of file dbap.h.

◆ b

struct { ... } b

◆ endinit

uint8_t endinit

Definition at line 389 of file dbap.h.

◆ reset

uint8_t reset

Definition at line 385 of file dbap.h.

◆ sup_err_dis

uint8_t sup_err_dis

Definition at line 387 of file dbap.h.

◆ w

uint8_t w

Definition at line 392 of file dbap.h.


The documentation for this union was generated from the following file: