ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_UF_REGION_W_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_UF_REGION_W_t:
Collaboration graph

Data Fields

struct {
   uint8_t   empty: 4
 
   uint8_t   region_load: 4
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 427 of file dbap.h.

Field Documentation

◆ b

struct { ... } b

◆ empty

uint8_t empty

Definition at line 429 of file dbap.h.

◆ region_load

uint8_t region_load

Definition at line 430 of file dbap.h.

◆ w

uint8_t w

Definition at line 432 of file dbap.h.


The documentation for this union was generated from the following file: