ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_COMMTYPE_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_COMMTYPE_t:
Collaboration graph

Data Fields

struct {
   uint8_t   commtype: 3
 
   uint8_t   _reserved_: 5
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 493 of file dbap.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 496 of file dbap.h.

◆ b

struct { ... } b

◆ commtype

uint8_t commtype

Definition at line 495 of file dbap.h.

◆ w

uint8_t w

Definition at line 498 of file dbap.h.


The documentation for this union was generated from the following file: