ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_TIMING_CFG_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_TIMING_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   ck_cal_en: 1
 
   uint8_t   _reserved1_: 2
 
   uint8_t   ck_cal_rst: 1
 
   uint8_t   osctrain_sel: 1
 
   uint8_t   _reserved2_: 3
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 590 of file dbap.h.

Field Documentation

◆ _reserved1_

uint8_t _reserved1_

Definition at line 593 of file dbap.h.

◆ _reserved2_

uint8_t _reserved2_

Definition at line 596 of file dbap.h.

◆ b

struct { ... } b

◆ ck_cal_en

uint8_t ck_cal_en

Definition at line 592 of file dbap.h.

◆ ck_cal_rst

uint8_t ck_cal_rst

Definition at line 594 of file dbap.h.

◆ osctrain_sel

uint8_t osctrain_sel

Definition at line 595 of file dbap.h.

◆ w

uint8_t w

Definition at line 598 of file dbap.h.


The documentation for this union was generated from the following file: