ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_SPI_CFG_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_SPI_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   spicrcseed: 4
 
   uint8_t   spi_crc_len: 2
 
   uint8_t   datasize: 1
 
   uint8_t   _reserved_: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 632 of file dbap.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 637 of file dbap.h.

◆ b

struct { ... } b

◆ datasize

uint8_t datasize

Definition at line 636 of file dbap.h.

◆ spi_crc_len

uint8_t spi_crc_len

Definition at line 635 of file dbap.h.

◆ spicrcseed

uint8_t spicrcseed

Definition at line 634 of file dbap.h.

◆ w

uint8_t w

Definition at line 641 of file dbap.h.


The documentation for this union was generated from the following file: