ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_DSP_CFG_U4_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_DSP_CFG_U4_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved0_: 2
 
   uint8_t   int_out: 1
 
   uint8_t   _reserved_: 5
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 753 of file dbap.h.

Field Documentation

◆ _reserved0_

uint8_t _reserved0_

Definition at line 755 of file dbap.h.

◆ _reserved_

uint8_t _reserved_

Definition at line 757 of file dbap.h.

◆ b

struct { ... } b

◆ int_out

uint8_t int_out

Definition at line 756 of file dbap.h.

◆ w

uint8_t w

Definition at line 759 of file dbap.h.


The documentation for this union was generated from the following file: