ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_DSP_CFG_U5_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_DSP_CFG_U5_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved_: 4
 
   uint8_t   st_ctrl: 4
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 782 of file dbap.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 784 of file dbap.h.

◆ b

struct { ... } b

◆ st_ctrl

uint8_t st_ctrl

Definition at line 785 of file dbap.h.

◆ w

uint8_t w

Definition at line 787 of file dbap.h.


The documentation for this union was generated from the following file: