ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_INT_CFG_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_INT_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   _reserved0_: 3
 
   uint8_t   int_polarity: 1
 
   uint8_t   int_ps: 2
 
   uint8_t   _reserved1_: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 818 of file dbap.h.

Field Documentation

◆ _reserved0_

uint8_t _reserved0_

Definition at line 820 of file dbap.h.

◆ _reserved1_

uint8_t _reserved1_

Definition at line 823 of file dbap.h.

◆ b

struct { ... } b

◆ int_polarity

uint8_t int_polarity

Definition at line 821 of file dbap.h.

◆ int_ps

uint8_t int_ps

Definition at line 822 of file dbap.h.

◆ w

uint8_t w

Definition at line 825 of file dbap.h.


The documentation for this union was generated from the following file: