ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXPS7250_DSP_STAT_t Union Reference

#include <dbap.h>

Collaboration diagram for FXPS7250_DSP_STAT_t:
Collaboration graph

Data Fields

struct {
   uint8_t   st_error: 1
 
   uint8_t   cm_error: 1
 
   uint8_t   st_active: 1
 
   uint8_t   st_incmplt: 1
 
   uint8_t   _reserved0_: 1
 
   uint8_t   pabs_low: 1
 
   uint8_t   pabs_high: 1
 
   uint8_t   _reserved1_: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 909 of file dbap.h.

Field Documentation

◆ _reserved0_

uint8_t _reserved0_

Definition at line 915 of file dbap.h.

◆ _reserved1_

uint8_t _reserved1_

Definition at line 918 of file dbap.h.

◆ b

struct { ... } b

◆ cm_error

uint8_t cm_error

Definition at line 912 of file dbap.h.

◆ pabs_high

uint8_t pabs_high

Definition at line 917 of file dbap.h.

◆ pabs_low

uint8_t pabs_low

Definition at line 916 of file dbap.h.

◆ st_active

uint8_t st_active

Definition at line 913 of file dbap.h.

◆ st_error

uint8_t st_error

Definition at line 911 of file dbap.h.

◆ st_incmplt

uint8_t st_incmplt

Definition at line 914 of file dbap.h.

◆ w

uint8_t w

Definition at line 920 of file dbap.h.


The documentation for this union was generated from the following file: