ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_STATUS_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xdr: 1
 
   uint8_t   ydr: 1
 
   uint8_t   zdr: 1
 
   uint8_t   zyxdr: 1
 
   uint8_t   xow: 1
 
   uint8_t   yow: 1
 
   uint8_t   zow: 1
 
   uint8_t   zyxow: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 100 of file fxls8471q.h.

Field Documentation

◆ b

struct { ... } b

◆ w

uint8_t w

Definition at line 119 of file fxls8471q.h.

◆ xdr

uint8_t xdr

Definition at line 102 of file fxls8471q.h.

◆ xow

uint8_t xow

Definition at line 110 of file fxls8471q.h.

◆ ydr

uint8_t ydr

Definition at line 104 of file fxls8471q.h.

◆ yow

uint8_t yow

Definition at line 112 of file fxls8471q.h.

◆ zdr

uint8_t zdr

Definition at line 106 of file fxls8471q.h.

◆ zow

uint8_t zow

Definition at line 114 of file fxls8471q.h.

◆ zyxdr

uint8_t zyxdr

Definition at line 108 of file fxls8471q.h.

◆ zyxow

uint8_t zyxow

Definition at line 116 of file fxls8471q.h.


The documentation for this union was generated from the following file: