ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_INT_SOURCE_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_INT_SOURCE_t:
Collaboration graph

Data Fields

struct {
   uint8_t   src_drdy: 1
 
   uint8_t   src_a_vecm: 1
 
   uint8_t   src_ff_mt: 1
 
   uint8_t   src_pulse: 1
 
   uint8_t   src_lndprt: 1
 
   uint8_t   src_trans: 1
 
   uint8_t   src_fifo: 1
 
   uint8_t   src_aslp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 427 of file fxls8471q.h.

Field Documentation

◆ b

struct { ... } b

◆ src_a_vecm

uint8_t src_a_vecm

Definition at line 431 of file fxls8471q.h.

◆ src_aslp

uint8_t src_aslp

Definition at line 443 of file fxls8471q.h.

◆ src_drdy

uint8_t src_drdy

Definition at line 429 of file fxls8471q.h.

◆ src_ff_mt

uint8_t src_ff_mt

Definition at line 433 of file fxls8471q.h.

◆ src_fifo

uint8_t src_fifo

Definition at line 441 of file fxls8471q.h.

◆ src_lndprt

uint8_t src_lndprt

Definition at line 437 of file fxls8471q.h.

◆ src_pulse

uint8_t src_pulse

Definition at line 435 of file fxls8471q.h.

◆ src_trans

uint8_t src_trans

Definition at line 439 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 446 of file fxls8471q.h.


The documentation for this union was generated from the following file: