ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_PL_STATUS_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_PL_STATUS_t:
Collaboration graph

Data Fields

struct {
   uint8_t   bafro: 1
 
   uint8_t   lapo: 2
 
   uint8_t   _reserved_: 3
 
   uint8_t   lo: 1
 
   uint8_t   newlp: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 605 of file fxls8471q.h.

Field Documentation

◆ _reserved_

uint8_t _reserved_

Definition at line 611 of file fxls8471q.h.

◆ b

struct { ... } b

◆ bafro

uint8_t bafro

Definition at line 607 of file fxls8471q.h.

◆ lapo

uint8_t lapo

Definition at line 609 of file fxls8471q.h.

◆ lo

uint8_t lo

Definition at line 612 of file fxls8471q.h.

◆ newlp

uint8_t newlp

Definition at line 614 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 617 of file fxls8471q.h.


The documentation for this union was generated from the following file: