ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_A_FFMT_CFG_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_A_FFMT_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   reserved: 3
 
   uint8_t   xefe: 1
 
   uint8_t   yefe: 1
 
   uint8_t   zefe: 1
 
   uint8_t   oae: 1
 
   uint8_t   ele: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 840 of file fxls8471q.h.

Field Documentation

◆ b

struct { ... } b

◆ ele

uint8_t ele

Definition at line 852 of file fxls8471q.h.

◆ oae

uint8_t oae

Definition at line 850 of file fxls8471q.h.

◆ reserved

uint8_t reserved

Definition at line 842 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 855 of file fxls8471q.h.

◆ xefe

uint8_t xefe

Definition at line 844 of file fxls8471q.h.

◆ yefe

uint8_t yefe

Definition at line 846 of file fxls8471q.h.

◆ zefe

uint8_t zefe

Definition at line 848 of file fxls8471q.h.


The documentation for this union was generated from the following file: