ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_TRANSIENT_CFG_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_TRANSIENT_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   hpf_byp: 1
 
   uint8_t   xtefe: 1
 
   uint8_t   ytefe: 1
 
   uint8_t   ztefe: 1
 
   uint8_t   ele: 1
 
   uint8_t   reserved: 3
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1043 of file fxls8471q.h.

Field Documentation

◆ b

struct { ... } b

◆ ele

uint8_t ele

Definition at line 1056 of file fxls8471q.h.

◆ hpf_byp

uint8_t hpf_byp

Definition at line 1045 of file fxls8471q.h.

◆ reserved

uint8_t reserved

Definition at line 1058 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 1061 of file fxls8471q.h.

◆ xtefe

uint8_t xtefe

Definition at line 1047 of file fxls8471q.h.

◆ ytefe

uint8_t ytefe

Definition at line 1050 of file fxls8471q.h.

◆ ztefe

uint8_t ztefe

Definition at line 1053 of file fxls8471q.h.


The documentation for this union was generated from the following file: