ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_PULSE_CFG_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_PULSE_CFG_t:
Collaboration graph

Data Fields

struct {
   uint8_t   xspefe: 1
 
   uint8_t   xdpefe: 1
 
   uint8_t   yspefe: 1
 
   uint8_t   ydpefe: 1
 
   uint8_t   zspefe: 1
 
   uint8_t   zdpefe: 1
 
   uint8_t   ele: 1
 
   uint8_t   dpa: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1253 of file fxls8471q.h.

Field Documentation

◆ b

struct { ... } b

◆ dpa

uint8_t dpa

Definition at line 1269 of file fxls8471q.h.

◆ ele

uint8_t ele

Definition at line 1267 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 1272 of file fxls8471q.h.

◆ xdpefe

uint8_t xdpefe

Definition at line 1257 of file fxls8471q.h.

◆ xspefe

uint8_t xspefe

Definition at line 1255 of file fxls8471q.h.

◆ ydpefe

uint8_t ydpefe

Definition at line 1261 of file fxls8471q.h.

◆ yspefe

uint8_t yspefe

Definition at line 1259 of file fxls8471q.h.

◆ zdpefe

uint8_t zdpefe

Definition at line 1265 of file fxls8471q.h.

◆ zspefe

uint8_t zspefe

Definition at line 1263 of file fxls8471q.h.


The documentation for this union was generated from the following file: