ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_PULSE_SRC_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_PULSE_SRC_t:
Collaboration graph

Data Fields

struct {
   uint8_t   polx: 1
 
   uint8_t   poly: 1
 
   uint8_t   polz: 1
 
   uint8_t   dpe: 1
 
   uint8_t   axx: 1
 
   uint8_t   axy: 1
 
   uint8_t   axz: 1
 
   uint8_t   ea: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1335 of file fxls8471q.h.

Field Documentation

◆ axx

uint8_t axx

Definition at line 1345 of file fxls8471q.h.

◆ axy

uint8_t axy

Definition at line 1347 of file fxls8471q.h.

◆ axz

uint8_t axz

Definition at line 1349 of file fxls8471q.h.

◆ b

struct { ... } b

◆ dpe

uint8_t dpe

Definition at line 1343 of file fxls8471q.h.

◆ ea

uint8_t ea

Definition at line 1351 of file fxls8471q.h.

◆ polx

uint8_t polx

Definition at line 1337 of file fxls8471q.h.

◆ poly

uint8_t poly

Definition at line 1339 of file fxls8471q.h.

◆ polz

uint8_t polz

Definition at line 1341 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 1354 of file fxls8471q.h.


The documentation for this union was generated from the following file: