ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_PULSE_LTCY_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_PULSE_LTCY_t:
Collaboration graph

Data Fields

struct {
   uint8_t   ltcy
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1540 of file fxls8471q.h.

Field Documentation

◆ b

struct { ... } b

◆ ltcy

uint8_t ltcy

Definition at line 1542 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 1545 of file fxls8471q.h.


The documentation for this union was generated from the following file: