ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_CTRL_REG1_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_CTRL_REG1_t:
Collaboration graph

Data Fields

struct {
   uint8_t   mode: 1
 
   uint8_t   f_read: 1
 
   uint8_t   lnoise: 1
 
   uint8_t   dr: 3
 
   uint8_t   aslp_rate: 2
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1618 of file fxls8471q.h.

Field Documentation

◆ aslp_rate

uint8_t aslp_rate

Definition at line 1628 of file fxls8471q.h.

◆ b

struct { ... } b

◆ dr

uint8_t dr

Definition at line 1626 of file fxls8471q.h.

◆ f_read

uint8_t f_read

Definition at line 1622 of file fxls8471q.h.

◆ lnoise

uint8_t lnoise

Definition at line 1624 of file fxls8471q.h.

◆ mode

uint8_t mode

Definition at line 1620 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 1632 of file fxls8471q.h.


The documentation for this union was generated from the following file: