ISSDK  1.8
IoT Sensing Software Development Kit
Data Fields
FXLS8471Q_CTRL_REG3_t Union Reference

#include <fxls8471q.h>

Collaboration diagram for FXLS8471Q_CTRL_REG3_t:
Collaboration graph

Data Fields

struct {
   uint8_t   pp_od: 1
 
   uint8_t   ipol: 1
 
   uint8_t   wake_en_a_vecm: 1
 
   uint8_t   wake_ff_mt: 1
 
   uint8_t   wake_pulse: 1
 
   uint8_t   wake_lndprt: 1
 
   uint8_t   wake_trans: 1
 
   uint8_t   fifo_gate: 1
 
} b
 
uint8_t w
 

Detailed Description

Definition at line 1750 of file fxls8471q.h.

Field Documentation

◆ b

struct { ... } b

◆ fifo_gate

uint8_t fifo_gate

Definition at line 1766 of file fxls8471q.h.

◆ ipol

uint8_t ipol

Definition at line 1754 of file fxls8471q.h.

◆ pp_od

uint8_t pp_od

Definition at line 1752 of file fxls8471q.h.

◆ w

uint8_t w

Definition at line 1769 of file fxls8471q.h.

◆ wake_en_a_vecm

uint8_t wake_en_a_vecm

Definition at line 1756 of file fxls8471q.h.

◆ wake_ff_mt

uint8_t wake_ff_mt

Definition at line 1758 of file fxls8471q.h.

◆ wake_lndprt

uint8_t wake_lndprt

Definition at line 1762 of file fxls8471q.h.

◆ wake_pulse

uint8_t wake_pulse

Definition at line 1760 of file fxls8471q.h.

◆ wake_trans

uint8_t wake_trans

Definition at line 1764 of file fxls8471q.h.


The documentation for this union was generated from the following file: